Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84708members
354091posts

macintosh 10.5.6 & surge protection

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
joselyca_apc
Cadet
0 Likes
1
202

macintosh 10.5.6 & surge protection

This was originally posted on APC forums on 5/29/2009


I have a 550 powerchute ES series connected to a macintosh system 10.5.6. I know there is now drive for this system and the system recognizes the APC but it doesn't do what it could be done if i could use the drive.

Do I still need to connect the surge via UBS to my computer? isn't enough to plug in there the computer and external HD? don't I have the same type of protection?


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
202

Re: macintosh 10.5.6 & surge protection

This reply was originally posted by Angela on APC forums on 5/29/2009


i am not sure what you mean to be honest.

if you dont install powerchute software, and want your system to shutdown gracefully, you need to configure some options in System Preferences->Energy saver to make sure your computer shuts down gracefully when the UPS runs out of battery power. it is not REQUIRED to do this for the UPS to provide surge protection and battery back up but it is required to have your computer shutdown gracefully.

see my attached instructions.

other than that i am not sure what you mean if you are able to clarify..

See Answer In Context

Attachments
1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
203

Re: macintosh 10.5.6 & surge protection

This reply was originally posted by Angela on APC forums on 5/29/2009


i am not sure what you mean to be honest.

if you dont install powerchute software, and want your system to shutdown gracefully, you need to configure some options in System Preferences->Energy saver to make sure your computer shuts down gracefully when the UPS runs out of battery power. it is not REQUIRED to do this for the UPS to provide surge protection and battery back up but it is required to have your computer shutdown gracefully.

see my attached instructions.

other than that i am not sure what you mean if you are able to clarify..

Attachments