apcupsd 3.14.14 not finding Back-UPS 550 on Mac OS 10.14.5

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • apcupsd 3.14.14 not finding Back-UPS 550 on Mac OS 10.14.5
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
Administrator BillP Administrator
2151
Teken
Kirk Teken
120
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
Solved Go to Solution
Back to APC UPS for Home and Office Forum
Start a Topic
Solved
Anonymous user
Not applicable

Posted: ‎2021-06-28 08:06 AM . Last Modified: ‎2024-03-26 03:41 AM

0 Likes
1
1319
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
Posted: ‎2021-06-28 08:06 AM . Last Modified: ‎2024-03-26 03:41 AM

apcupsd 3.14.14 not finding Back-UPS 550 on Mac OS 10.14.5

Hi, I have a Back-UPS 550 that I'd like to use to shut down two computers when the power goes out. I installed apcupsd 3.14.14 from http://www.apcupsd.org/ on the same Mac to which the Back-UPS is connected (via USB) and checked that /etc/apcupsd/apcupsd.conf is appropriately configured. The defaults seem sane:

UPSCABLE usb
UPSTYPE usb
DEVICE
LOCKFILE /var/tmp
SCRIPTDIR /etc/apcupsd
PWRFAILDIR /etc/apcupsd
NOLOGINDIR /etc
ONBATTERYDELAY 6
BATTERYLEVEL 5
MINUTES 3
TIMEOUT 0
ANNOY 300
ANNOYDELAY 60
NOLOGON disable
KILLDELAY 0
NETSERVER on
NISIP 0.0.0.0
NISPORT 3551
EVENTSFILE /var/log/apcupsd.events
EVENTSFILEMAX 10

Yes, I gave the developer permission in System Preferences / Security & Privacy / General / Allow...

According to the docs, a simple kext is supposed to prevent Mac OS from finding the UPS and showing it under Energy Saver / UPS. However it still shows up under Shutdown Options as Back-UPS ES 550G FW:904.W1 .D USB FW:W1. I also checked, and though the kext is installed in /System/Library/Extensions/ApcupsdDummy.kext, kextstat doesn't show it as loaded. I also tried forcing it to load with sudo kextload. It still doesn't appear in kextstat -l. So I'm guessing there's a problem with the kext.

apcagent shows up in the status line with a red ?, shows UPS: , and under status shows STATUS: COMMLOST. 

Each reboot, an additional "Communications with UPS lost." appears under Events.

It seems that Mac OS is grabbing the USB connection to the Back-UPS, which prevents apcupsd from connecting to it.

Not sure if related, but Mac OS also warned that either apcupsd or apcagent would not be compatible with a future Mac OS version. They probably need to be built with a newer Xcode.

Any ideas? thanks

Labels
  • Labels:
  • Back-UPS & Surge Protectors
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-06-28 08:06 AM . Last Modified: ‎2024-03-26 03:41 AM

0 Likes
0
1319
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
Posted: ‎2021-06-28 08:06 AM . Last Modified: ‎2024-03-26 03:41 AM

Hi,

I recommend checking the APCUPSD mail list. http://www.apcupsd.org/wordpress/email-lists/

If needed you can request assistance there of others that are running Mac OSX 10.14 with APCUPSD. 

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-06-28 08:06 AM . Last Modified: ‎2024-03-26 03:41 AM

0 Likes
0
1320
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
Posted: ‎2021-06-28 08:06 AM . Last Modified: ‎2024-03-26 03:41 AM

Hi,

I recommend checking the APCUPSD mail list. http://www.apcupsd.org/wordpress/email-lists/

If needed you can request assistance there of others that are running Mac OSX 10.14 with APCUPSD. 
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.