Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

SMT and SUA 3000i with NMC2 Query

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • SMT and SUA 3000i with NMC2 Query
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2150
Teken
Teken
144
Techie_apc
Techie_apc
83
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
Back to APC UPS for Home and Office Forum
Start a Topic
ianj7777_apc
ianj7777_apc
Explorer

Posted: ‎2022-03-24 02:50 AM

0 Likes
1
1030
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
Posted: ‎2022-03-24 02:50 AM

SMT and SUA 3000i with NMC2 Query

Hi All

 

I'm sure this is a really silly question but nevertheless here goes.

 

I want to connect an SMT3000i to one of our servers then use Powerchute BE to shutdown this and another server.

 

I can see the NMC2 using a browser and set the basic options over the web interface, no idea if this is as good as Powerchute or just a more basic option.

 

However I have plugged in the USB lead from the server into the RJ45 directly on the UPS and a separate lead from a network switch into the NMC2 RJ45 port, is this correct?

 

Powerchute cannot communicate with the UPS so I guess I've done something wrong.

 

I also need the same setup for a different installation in a different building using and SUA3000i. I note there is a different lead p/no for the SUA USB to RJ45 for some reason.

 

As I said if this is a silly question I apologise but I cannot seem to find where it states what needs to connect where, stuck for time as well as I go on leave from tomorrow night.

 

Any help appreciated.

 

Thanks

 

Ian Jones

Labels
  • Labels:
  • Home & Office - UPS & Software
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
BillP
BillP Leader
Leader

Posted: ‎2022-04-05 11:00 AM

0 Likes
0
940
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
Posted: ‎2022-04-05 11:00 AM

@ianj7777_apc 

 

Do both UPS have network management cards (NMC) installed? If so you can install PowerChute Network Shutdown on each server and gracefully power them off via the NMC. 

 

If the UPS do not have NMCs you can install PowerChute Business Edition on one of the server. You will need to connect the USB cable or Serial cable that shipped with UPS to the server for communications. For the second sever write a script that PowerChute will use to send a shutdown signal to the second server. 

  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.