Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Problem with MikroTik and UPS APC Backup BX1600MI-GR

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • Problem with MikroTik and UPS APC Backup BX1600MI-GR
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
BillP Leader
2151
Teken
Teken
152
Techie_apc
Techie_apc
83
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
Back to APC UPS for Home and Office Forum
Start a Topic
ianiovski
ianiovski
Explorer

Posted: ‎2024-01-21 08:32 AM . Last Modified: ‎2024-01-21 08:33 AM

0 Likes
1
1177
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
Posted: ‎2024-01-21 08:32 AM . Last Modified: ‎2024-01-21 08:33 AM

Problem with MikroTik and UPS APC Backup BX1600MI-GR

Hello, I have a monitoring problem between RB960PGS and UPS APC BX1600MI-GR. The router sees the UPS and shows its parameters, but in the Mikrotik logs it constantly spits out UPS Power on and then Power off for a minute. I think that the problem is something in the communication, because the USB of UPS is 1.10, and of RB it is 2.0. I read in the forum, the communication problem was solved with a simple Usb Hub 2.0, I bought one, but the result is the same. I wanted to have monitoring on it, and that was one of my important requirements when buying the UPS, but that's exactly what didn't work as it should. 

 

 

Capture.png

 

 

 

Labels
  • Labels:
  • Back-UPS & Surge Protectors
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Teken
Teken
Champion

Posted: ‎2024-01-22 09:00 AM

0 Likes
0
1163
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
Posted: ‎2024-01-22 09:00 AM

Can you provide some images of what you see from the router?!? Also, how does the router communicate with the UPS?!? Are you using a third party application like APCUPSD, NUT, WinPower, Other? To have a base line I would install Power Chute Personal Edition (PCPE) on to a computer and see how it behaves.

 

If you see no problems this affirms the cable and the UPS is operating as intended. If it doesn't operate as expected than you found your problem(s) because its either the cable, UPS, Both. If we just assume it works perfectly fine using PCPE software while connected to a computer. The most common issues I've seen with third party UPS applications are drivers. Next, is selecting the wrong type of connection whether it be USB, Network, SNMP, etc.

 

It goes without saying defining the type of UPS and how its interconnected (USB / Network) in the application is paramount in hopes of seeing success. Given, you obviously have a connection and see something in the Router it could be just a timing issue that needs to be adjusted in whatever software you're using to connect to the APC UPS.

 

Just so you know I can't see any image you've posted besides a triangle box! ☹️
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.