Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84505members
353724posts

PowerChute not shutting down automatically when power lost during PC boot

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

mhuhn_apc
Cadet
0 Likes
0
74

PowerChute not shutting down automatically when power lost during PC boot

This was originally posted on APC forums on 12/16/2016


I have a Back UPS CS650 connected via USB to my Windows 8.1 PC in order to let PowerChute Personal Edition 3.0.2 shut the PC down (or actually hibernate) when power was lost. A few minutes later it goes to battery sleep and will wake up again when external power returns. After wake up, PC will automatically boot. That works fine. However, in one case this doesn't work.

To reproduce the problem, I do the following:

  1. Take away external power for 5 minutes so that PC is in hibernate, UPS is in battery sleep
  2. Provide external power again temporarily (for 8 seconds) so that PC gets power again and is booted (or starts restoring from hibernate)
  3. Take external power away while PC is restoring from Hibernate, so that there is no power at the point in time when Windows continues to run
  4. After Windows has restored, PowerChute shows me a system tray message that it will shut down the PC again in 1 minute. This is exactly what I want

The problem is: it doesn't do it. The PC stays on and the Back UPS runs on battery permanently. To me it seems like a bug in PowerChute. What can I do?