I want it to stay on after it turns off PC via Powerchute

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • I want it to stay on after it turns off PC via Powerchute
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
Administrator BillP Administrator
2151
Teken
Kirk Teken
123
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
Back to APC UPS for Home and Office Forum
Start a Topic
RichardOtter
Crewman RichardOtter
Crewman

Posted: ‎2024-05-02 05:44 PM

0 Likes
2
666
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
Posted: ‎2024-05-02 05:44 PM

I want it to stay on after it turns off PC via Powerchute

I have a Back UPS Pro 1500 S and have installed Powerchute serial v1.2 on my Windows PC.

The UPS powers the PC and a router/ONT and network switches.

In case of mains power outage, I want Powerchute to tell the computer to hibernate after 1 minute, but I want the UPS to continue to supply power so the attached network devices remain on.

How do I do it?

 

 

 

Labels
  • Labels:
  • Home & Office - UPS & Software
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
RyanG32
Ensign RyanG32 Ensign
Ensign

Posted: ‎2024-11-10 02:24 PM

0 Likes
0
526
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
Posted: ‎2024-11-10 02:24 PM

There are a couple of ways of implementing this This may also vary depending on the model of the UPS

First you need to choose the option to not shutdown n event of a power outtage

RyanG32_0-1731275198656.png

Then  create a batch file .bat  with either command will depend on which works with your operating system

Configuring Command Files for use with Powerchute Business Edition - APC USA

Using the shutdown command: Type `shutdown /h

Using powercfg.exe: Type `powercfg.exe /hibernate 

save the batch file and see if you can run it and if it is able to hibernate your computer

if it works

then Go to Power Chute > Event Configuration and choose the event that you want to trigger Hibernation and navigate to where the save batch file is

 

 

RyanG32_1-1731276339993.png

The problem with this setup is the automatic start ups sequence will not work since it needs to turn off output and when power comes back in turn on output  so Computer can be signalled to turn on

 

You can also uninstall PowerChute and use the native shutdown feature of the Computer this requires that the UPS is considered as a APC UPS or APC Battery BackUPS. and not a HID UPS which ,may require the driver to be reactivated

 

Video: What to do if the system is missing native shutdown battery options / How to restore HID UPS ...

 

 

 

Reply

Link copied. Please paste this link to share this article on your social media post.

fredkm
Lieutenant fredkm Lieutenant
Lieutenant

Posted: ‎2024-11-15 03:22 AM

0 Likes
0
506
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
Posted: ‎2024-11-15 03:22 AM

The new 1.3 version, scheduled for release later this month, will have an option for not shutting down the UPS after OS shutdown (only for Back-UPS models).

 

Note that if you have configured your PC to automatically turn on on AC power recovery, this obviously will no longer work. This relies on the UPS automatically turning on when AC power returns. Using the new option, the UPS (powering your PC) doesn't turn off and on, and the PC will not detect AC power recovery.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.