Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84584members
353853posts

Can I use a a Back UPS RS 1500 just for it's power conditioner / AVR without any batteries?

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
BillP
Administrator Administrator
Administrator
0 Likes
1
102

Can I use a a Back UPS RS 1500 just for it's power conditioner / AVR without any batteries?

This question was originally posted by insoc on APC forums on 5/17/2014


The batteries of my RS 1500 UPS died after 4 years. I replaced my UPS with a Pro 1500 and do not intend to buy expensive batteries to replace the old RS 1500 ones. I love UPS like the RS 1500 for it's power conditioner / AVR features so my question is if I can still use the RS 1500 as that without installing any new batteries and removing the old ones. If so, any way to stop all the alerts from sounding? Thanks a lot!


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
102

Re: Can I use a a Back UPS RS 1500 just for it's power conditioner / AVR without any batteries?

This reply was originally posted by Angela on APC forums on 5/19/2014


I think you can do this but the UPS may periodically turn off when there is a power event - where it'd normally transfer to battery and back online. Without the battery, the UPS will require you to manually turn it back on afterwards. I also don't know of a way (without opening the unit and modifying it at your own risk) to disable the "battery disconnect" chirp that you'll see along with a flashing replace battery LED.

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
103

Re: Can I use a a Back UPS RS 1500 just for it's power conditioner / AVR without any batteries?

This reply was originally posted by Angela on APC forums on 5/19/2014


I think you can do this but the UPS may periodically turn off when there is a power event - where it'd normally transfer to battery and back online. Without the battery, the UPS will require you to manually turn it back on afterwards. I also don't know of a way (without opening the unit and modifying it at your own risk) to disable the "battery disconnect" chirp that you'll see along with a flashing replace battery LED.