Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Back-UPS Pro 550 data port connections

APC UPS for Home and Office Forum

Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
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
  • APC UPS, Critical Power, Cooling and Racks
  • APC UPS for Home and Office Forum
  • Back-UPS Pro 550 data port connections
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BillP
Administrator BillP Administrator
2150
Teken
Kirk Teken
127
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
Solved Go to Solution
Back to APC UPS for Home and Office Forum
Start a Topic
Solved
Anonymous user
Not applicable

Posted: ‎2021-06-28 01:45 AM . Last Modified: ‎2024-03-27 03:18 AM

0 Likes
1
2170
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
Posted: ‎2021-06-28 01:45 AM . Last Modified: ‎2024-03-27 03:18 AM

Back-UPS Pro 550 data port connections

I have my UPS to safe guard my Synology 214Play from power outs which recently cost me the replacement of a 3tb drive along with a lot aggravation and time getting the system up to speed again.

So I purchased the UPS and all is running fine. My question is can I somehow can I somehow configure it so that I can configure it so that the data port is connected to my win7 pc that is running "Power Chute Personal Edition" and my NAS at the same time? At the moment it is one or the other. Is it possible to split the "Data Port" to run two cables? When the data port is connected to the NAS it sees it in its control screen and all is set up perfectly but then of course the "Power Chute" is not working so I then have to disconnect the data cable from the NAS and then connect to my pc. When I do this the NAS complains that it is disconnected which is correct.

I await your reply and help.

Many thanks

Labels
  • Labels:
  • Back-UPS & Surge Protectors
  • Tags:
  • 550
  • back-ups
  • pro
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-06-28 01:45 AM . Last Modified: ‎2024-03-27 03:18 AM

0 Likes
0
2170
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
Posted: ‎2021-06-28 01:45 AM . Last Modified: ‎2024-03-27 03:18 AM

For any Back-UPS UPS, this is not something we've tested or supported unfortunately. I imagine it might also require some type of modified cable and the Back-UPS may not be able to supply signals over it properly with its native chipset. Back-UPS products typically only support one data connection to one device at a time. A higher end UPS like a Smart-UPS supports USB, serial, and SmartSlot connectivity (on most models). Some NAS systems support USB or sometimes SNMP monitoring too so with a higher end UPS, you might be able to run two data connections to it simultaneously. Otherwise, it will have to be one or the other.

The other idea may be to use the UPS with the computer and depending on connection and how your NAS works, see if it is possible for your computer to issue a command or run a script to shut the NAS off instead of being directly connected to the UPS.

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-06-28 01:45 AM . Last Modified: ‎2024-03-27 03:18 AM

0 Likes
0
2171
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
Posted: ‎2021-06-28 01:45 AM . Last Modified: ‎2024-03-27 03:18 AM

For any Back-UPS UPS, this is not something we've tested or supported unfortunately. I imagine it might also require some type of modified cable and the Back-UPS may not be able to supply signals over it properly with its native chipset. Back-UPS products typically only support one data connection to one device at a time. A higher end UPS like a Smart-UPS supports USB, serial, and SmartSlot connectivity (on most models). Some NAS systems support USB or sometimes SNMP monitoring too so with a higher end UPS, you might be able to run two data connections to it simultaneously. Otherwise, it will have to be one or the other.

The other idea may be to use the UPS with the computer and depending on connection and how your NAS works, see if it is possible for your computer to issue a command or run a script to shut the NAS off instead of being directly connected to the UPS.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.