Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84598members
353864posts

BX1500 cycles rapidly between on line and on battery

APC UPS for Home and Office Forum

Schneider Electric support forum for our APC offers including Home Office UPS, Surge Protectors, UTS, software and services and associated products designed to share knowledge, installation, and configuration.

Solved
jeffn_apc
Cadet
0 Likes
1
112

BX1500 cycles rapidly between on line and on battery

This was originally posted on APC forums on 8/28/2012


Hi. My BX1500 UPS started cycling between on line and on battery. It switches back and forth rapidly -- maybe once per second or thereabouts. Neither the overload nor replace battery lights are lit. The UPS continues cycling even if I disconnect all loads. If I leave it plugged in and turn it off, it does not cycle.

If the unit is plugged in and turned on, and I unplug the AC power cord, the unit stops cycling and switches to on battery and stays there steady until I plug the AC cord back in, and then the unit goes back to the rapid cycling.

Any ideas what might cause the cycling? I searched this forum and google searched, but can't find anything other than one speculation that the battery might be bad. Could it be the battery even though the replace battery light is not on?

Thanks.

Message was edited by: jeffn Added a little more detail.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
111

Re: BX1500 cycles rapidly between on line and on battery

This reply was originally posted by Chris on APC forums on 8/28/2012


It may be doing this due to dirty power or low/high input voltage. Which Bx1500 do you have? You can try to change the sensitivity to see if this helps and we can check the voltage to see if it's a voltage issue. Depending on the model you have, the procedure for getting this info will be different. It will show a model # on a white sticker on the unit. It will likely be bx1500 or bx1500g. I have listed links to the manuals for each unit below. They show the procedure for changing the sensitivity for each.


http://www.apcmedia.com/salestools/ASTE-6Z7V72_R0_EN.pdf BX1500

http://www.apcmedia.com/salestools/EALN-7SEGRP_R6_EN.pdf BX1500g

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
112

Re: BX1500 cycles rapidly between on line and on battery

This reply was originally posted by Chris on APC forums on 8/28/2012


It may be doing this due to dirty power or low/high input voltage. Which Bx1500 do you have? You can try to change the sensitivity to see if this helps and we can check the voltage to see if it's a voltage issue. Depending on the model you have, the procedure for getting this info will be different. It will show a model # on a white sticker on the unit. It will likely be bx1500 or bx1500g. I have listed links to the manuals for each unit below. They show the procedure for changing the sensitivity for each.


http://www.apcmedia.com/salestools/ASTE-6Z7V72_R0_EN.pdf BX1500

http://www.apcmedia.com/salestools/EALN-7SEGRP_R6_EN.pdf BX1500g