Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-2904:21 AM. Last Modified: 2024-03-2212:51 AM
BX1300G UPS and it is unable to start PC
I have a BX1300G UPS and it is unable to start PC. For example, UPS been plugged into utility power for over 4 weeks. Only PC plugged in master outlet. I unplug UPS from utility power and PC turns off and starts to power up and then after 1 to 2 seconds powers off again and keeps cycling on and off. The runtine on battery UPS is 40 minutes or so per UPS. THe load level is 10% of battery capacity and the nominal power draw is 80 watts when running. Please help. The system has a F05 and F06 system fault. For the case I just described the USB was disconnected and the APC drivers were disabled and powerchute software uninstalled. I have also installed powerchute software and enable drivers all looks good and PC see UPS powerlevels etc... however the PC reboots when system test run in Powerchute and after reboot the test status is still never stated and has no indication of what happened. It seems like the PC startup surge current from the PC causes the UPS to reset and it never gets out of the loop. Please help.
Processor Intel(R) Core(TM) i7 CPU 920 @ 2.67GHz
Memory (RAM) 6.00 GB 7.5
Graphics ATI Radeon HD 4300/4500 Series 3.5
Gaming graphics 3323 MB Total available graphics memory 5.8
Primary hard disk 276GB Free (457GB Total) 5.9
Windows 7 Ultimate (64 bit)
System
Manufacturer DELL Inc.
Model Studio XPS 435T/9000
Total amount of system memory 6.00 GB RAM
System type 64-bit operating system
Number of processor cores 4
Storage
Total size of hard disk(s) 923 GB
Disk partition (C:) 276 GB Free (457 GB Total)
Media drive (D:) CD/DVD
Disk partition (E:) 104 GB Free (466 GB Total)
Graphics
Display adapter type ATI Radeon HD 4300/4500 Series
Total available graphics memory 3323 MB
Dedicated graphics memory 512 MB
Dedicated system memory 0 MB
Shared system memory 2811 MB
Display adapter driver version 8.753.0.0
Primary monitor resolution 1920x1080
Secondary monitor resolution 1440x900
DirectX version DirectX 10
Network
Network Adapter Realtek PCIe GBE Family Controller