Posted: 2021-06-28 05:00 AM . Last Modified: 2024-03-27 01:19 AM
BOSE and APC UPS BX650LI-MS
I just wanna ask the APC Guys here if my Connection below is Correct wherein i've Connected BOSE Companion to BX650LI
Is my Precious BOSE Speakers can be protected by APC?
Mostly here is my Connection wherein this is the electric flow Scenario:
220volts going to Surgeprotector P5-VN going to AVR 500watts Servo Motor with voltmeter going to UPS BX650LI-MS then to PC & BOSE
I've use a SERVO MOTOR AVR (FUSE TYPE) so that it can regulate MORE the current....Mostly, it has an Analog Voltmeter wherein you can see the current flow wherein Analog is more Accurate rather than Digital (According to Electrical People i've talked before)
Sad to say most APC home UPS don't have Servo Motor or a Voltmeter 😞 ........
I hope APC Experts can give me an advice and opinions with the picture above?
FYI, The White cable that is connected to P5-VN is an Electric Fan:-) is this Safe too?
Hope to hear from you.....
Thanks!
Marvin
- Labels:
-
Back-UPS & Surge Protectors
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
Posted: 2021-06-28 05:00 AM . Last Modified: 2024-03-27 01:19 AM
Hi,
We do not recommend plugging a UPS into anything other than the wall outlet but you can set the system up as you please. As for the Bose adapter, that is fine plugging it into the UPS.
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
Posted: 2021-06-28 05:00 AM . Last Modified: 2024-03-27 01:19 AM
Hi,
We do not recommend plugging a UPS into anything other than the wall outlet but you can set the system up as you please. As for the Bose adapter, that is fine plugging it into the UPS.
Link copied. Please paste this link to share this article on your social media post.