Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Search in
Posted: 2021-06-29 02:39 AM . Last Modified: 2024-03-22 02:23 AM
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 02:39 AM . Last Modified: 2024-03-22 02:23 AM
Folks,
I recently purchased a NS 1250 at Sam's Club (model #BN1250G). This UPS has a nice front LCD panel, and also features a "green" master outlet/slave outlets (when the device on the master is powered down, the UPS removes power to the slave outlets).
I bought this unit for use with a Linux box (CentOS 5.4). Of course, the PowerChute software that APC provides is only for Windows. (But now that I think of it, I did not get a CD with the BN1250G UPS). So I cannot use PowerChute.
I am sure on this forum that you have heard of APCUPSD , a software package which provides an interface to APC UPS's for UNIX-based operating systems.
For the most part, this UPS with APCUPSD works OK. With "apcaccess" I can get information about the UPS, such as model, serial #, battery capacity, load capacity, etc. And with "apctest", I can set the sensitivity, hi/lo transfer voltages, test the alarm, view/change battery date, view manufacturing date, turn off the alarm, etc. But two things that I cannot do with that I have done with another APC UPS via APCUPSD was to initiate a self-test, and perform a battery calibration.
I can initiate a self-test via the front panel (hold the power button for 6 seconds), but not via USB.
Does anyone know if this UPS supports a USB initiated self-test? I.E., can anyone with this connected to a Windows box initiate a self-test? I have a two-year old NS 1250 (the shorter model with the LCD), and it can do a self-test from the PowerChute 2.0 software I have (I am still using Windows 2000, so 2.0 is a new as I can get).
Also, does anyone know if the BN1250G supports USB initiated battery calibration? Truth be told, I have never seen mention of battery calibration till I started using APCUPSD.
Any thoughts/suggestions would be appreciated.
Thanks!
The Nth Traveler
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 02:39 AM . Last Modified: 2024-03-22 02:23 AM
I honestly don't own one of these units to answer your first question, but as far as I know it should support a self-test via USB. Not 100% sure though.
In regard to the calibration, that's not really a function for the Back-UPS units. PowerChute Personal Edition doesn't have this feature since it isn't commonly used outside of the Smart-UPS family. Realistically you only want to run a calibration when your expected runtime is way off, since it causes additional wear & tear on the battery. The Back-UPS units use simple signaling though, so it isn't uncommon to see weird expected runtimes on occasion, and that certainly wouldn't be remedied with a calibration.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 02:39 AM . Last Modified: 2024-03-22 02:23 AM
I honestly don't own one of these units to answer your first question, but as far as I know it should support a self-test via USB. Not 100% sure though.
In regard to the calibration, that's not really a function for the Back-UPS units. PowerChute Personal Edition doesn't have this feature since it isn't commonly used outside of the Smart-UPS family. Realistically you only want to run a calibration when your expected runtime is way off, since it causes additional wear & tear on the battery. The Back-UPS units use simple signaling though, so it isn't uncommon to see weird expected runtimes on occasion, and that certainly wouldn't be remedied with a calibration.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.