APC Back-UPS BX1600MI Charging Inconsistencies and High-Frequency Noise When Off
APC UPS for Home and Office Forum
Support forum to share knowledge about installation and configuration of APC offers including Home Office UPS, Surge Protectors, UTS, software and services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-01-1704:54 AM
APC Back-UPS BX1600MI Charging Inconsistencies and High-Frequency Noise When Off
Hi,
I just bought a new BX1600MI ups with a battery date of September 2024. Charged it about 24 hours and plugged my medium-range home PC on it; the PowerChute software showed 90% and after some time 99%. It never attained 100% even after shutting off the ups. The ups works fine and after a power outage of 2 minutes it only goes down 2 or 3%, so no problem here, but it never recharges back to 100%, only to 99%, EXCEPT if I unplug the USB data cable and either connect it again to the same port or to another one. Then it immediately goes to 100%, but during the same session if the electricity goes off let's say to 97%, same issue, only 99%. Also in the morning when I turn it on it says 80%, so I remove the data cable, reconnect it, and boom 100%. The same applies when I log in to my linux machine (not powerchute, but apcupsd).
The other issue is that when the UPS is off but connected, it emits a very high frequency sound (I can't hear it, only my kids can); is this a problem?
Other than these two issues, everything works normally (no heat, no blinking, no red lights, fast recharge, etc.),