how can i query status of the ups device from c++ program ?
APC UPS Data Center & Enterprise Solutions Forum
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2021-07-0104:16 AM. Last Modified: 2024-03-0502:24 AM
how can i query status of the ups device from c++ program ?
hello, i need some help with the APC SMT750i . it is connected to a standard PC which is part of a machine. PowerChute is installed and working. But i need to query the status of the ups from another program which is c++ and if the power fails than to move some part in the machine. can i use the serial rs232 cable connector (COM1) to send a query to the ups? and if so do i have to use the modbus protocol and how is the appropriate command ? i have tried sending different commands to the ups but i dont get a response so far. thank u for help