Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Any UPS that connects to the APC cloud will have the C prefix in the model number. If the UPS is model SMT750RM2UC then it will connect to the SmartConnect cloud. If is SMT or SMX750RM without the C prefix then it will not connect.
Note: if the model number ends in NC then then the UPS has a network card installed. The NC prefix indicates the UPS ships with a pre-installed network card and would not be a Smart Connected UPS. You can install a network card in a Smart Connected UPS but they do not ship with pre-installed network cards.
Any UPS that connects to the APC cloud will have the C prefix in the model number. If the UPS is model SMT750RM2UC then it will connect to the SmartConnect cloud. If is SMT or SMX750RM without the C prefix then it will not connect.
Note: if the model number ends in NC then then the UPS has a network card installed. The NC prefix indicates the UPS ships with a pre-installed network card and would not be a Smart Connected UPS. You can install a network card in a Smart Connected UPS but they do not ship with pre-installed network cards.