Unable to turn on the UPS after the firmware update
APC UPS Data Center & Enterprise Solutions Forum
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2024-12-0306:31 PM
This happens when the wrong firmware is uploaded or if the firmware gets damaged while being transferred over the network. We usually recommend that the firmware be updated with the advice of a representative and to use the firmware update wizard since it will detect the correct firmware and and the transfer is thru USB or serial which is less prone to data loss than over the network
How do I update the firmware of my CSH, SCL, SMC, SMT, SMTL, SMX, SRT, SRTL, XP and XU series Smart-UPS using the Firmware Upgrade Wizard?
If it still does not work check if the unit still has a warranty otherwise you may want to purchase a new UPS
You can swap your existing unit (Upgrade for a Smart UPS or Symmetra Single Phase UPS unit) at a significant discount. Free return shipping label on trade in.
The Benefits of Trade UPS: >> Purchase new/most updated unit at a discounted price >> We will send an APC prepaid return shipping label >> Trade up to 4x current VA capacity (adding onto load) >> Renewed warranty (factory warranty of 2 or 3 years depending on the unit) >> Option for extended warranty (additional 1 or 3 years)