Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Search in
Free
EnglishStrengthen your foundational knowledge in Data Centers for free, enroll in this path today and start your learning journey!
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-28 10:48 AM . Last Modified: 2024-03-15 05:48 AM
Hello Everyone,
Long time reader, have not posted anything as of yet on the forum. I have a question now that I cannot seem to find an answer for at all.
I have had and used, for many years an APC Smart-UPS 1000I NET with serial number GS9814430025. For reference, it has an AP9631 NMC2 Rhodes in it. I recently had to replace the batteries, as the cells that were in the unit started going towards the end of their useful life. In replacing the batteries, I reset the battery constant values in the EEPROM, and somehow pressed the dreaded Ctrl-Y in the tty session, clearing the EEPROM.
I was, subsequently, able to restore the values of the EEPROM, at least as far as I can pick up, correctly. And herein the question. Would anyone that have one of these units be able to extract the EEPROM values for me from their unit, for verification, please? I would be interested in comparing the values of a SUA 1000I NET also, as I think these values may be close or the same.
Here are the values that I currently have captured (as extracted with APCUPSD):
"
1) Query the UPS for all known values
2) Perform a Battery Runtime Calibration
3) Abort Battery Calibration
4) Monitor Battery Calibration progress
5) Program EEPROM
6) Enter TTY mode communicating with UPS
Q) Quit
Select function number: 1
I am going to run through the series of queries of the UPS
that are used in initializing apcupsd.
Simulating UPSlinkCheck ...
Wrote: Y Got: SM
Attempting to use smart_poll() ...
Sent: Y Got: SM Good -- smart_poll() works!.
Going to ask for valid commands...
Wrote: a Got: 3.?=.-789>@ABCDEFGKLMNOPQRSUVWXYZ'abcefgjklmnopqrsuxyz~
Protocol version is: 3
Alert characters are: ?=
Command characters are: ^A^N^Z-789>@ABCDEFGKLMNOPQRSUVWXYZ'abcefgjklmnopqrsuxyz~
Now running through apcupsd get_UPS capabilities().
NA indicates that the feature is Not Available
UPS Status: 08
Line quality: FF
Reason for last transfer to batteries: S
Self-Test Status: NO
Line Voltage: 231.4
Line Voltage Max: 231.4
Line Voltage Min: 230.1
Output Voltage: 231.4
Batt level percent: 079.0
Batt voltage: 28.14
UPS Load: 000.0
Line freq: 50.00
Runtime left: 0287
UPS Internal temp: 028.8
Dip switch settings: 00
Register 1: 00
Register 2: 00
Register 3: 00
Sensitivity: H
Wakeup delay: 000
Sleep delay: 020
Low transfer voltage: 196
High transfer voltage: 253
Batt charge for return: 00
Alarm status: N
Low battery shutdown level: 02
UPS Name: UPS_IDEN
UPS Self test interval: 336
UPS manufacture date: 04/01/98
UPS serial number: GS9814430025
Date battery replaced: 12/09/19
Output voltage when on batteries: 230
Nominal battery voltage: 024
Percent humidity: NA
Ambient temperature: NA
Firmware revision: 60.9.I
Number of external batteries installed: 000
Number of bad batteries installed: NA
UPS model as defined by UPS: SMART-UPS 1000
UPS EPROM capabilities string: uD43132135138129uM43229234239224uA43110112114108uI43253264271280lD43103100097106lM43177172168182lA43090092081085lI43196188208204e44200155090oI43230240220225oD13115oJ13100oM13208s441HMLLq44202050710p443020180300600k4410TLNr443000060180300E443336168ON OFF
The EPROM string is 253 characters long!
Hours since last self test: NA
That is all for now.
"
I attach here the following:
Image with model and serial numbers
Image of front of unit
TL;DR
Would anyone that have one of these units be able to extract the EEPROM values possibly for me from their unit, for verification, please?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-28 10:48 AM . Last Modified: 2024-03-15 05:48 AM
Anyone?
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.