Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Search in
Free
EnglishStrengthen your foundational knowledge in Data Centers for free, enroll in this path today and start your learning journey!
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-09-13 08:45 AM . Last Modified: 2023-10-11 12:38 AM
Hi,
I bought an SMT750IC and have it up and working with SmartConnect which is actually better than I thought it would be though still very limited. Updating the firmware from the cloud was useful, especially as I have no Windows machine.
I also got it working with APCUPSD using the included USB cable and ModBus connected to a Mac, the working apcupsd .conf was this:
UPSCABLE usb
UPSTYPE modbus
DEVICE
Though seriously, why a double-ended USB-A cable and not the usual USB A>B ????
Anyway, in the latest Firmware 4.1 release notes of the SMT750IC it says "SMT series now supports Modbus over TCP" and they are talking about the embedded SmartConnect port.
And in the updated user manual it now details the options that are in the advanced settings of the UPS:
- Slave ID 1 1- 223 Sets the Modbus slave address of UPS
- Ser+USB - Enables or disables UPS Modbus protocol over serial and USB ports [This was by default disabled, I had to enable it to get Modbus working over USB to apcupsd]
- TCP Protocols - Enables or disables UPS Modbus TCP/IP protocol provided by the embedded SmartConnect port.
OK, so according to this it is now opening MODBUS protocol through the SmartConnect ethernet port. And APCUPSD understands MODBUS protocol.
So is there any chance to connect APCUPSD to the UPS over the network to the SmartConnect port using MODBUS protocol? If so any idea how? If not, then how would you use this Modbus-over-TCP feature?
Thanks.
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
Posted: 2022-04-25 03:27 AM
@PVasileff- I'm afraid I never got anywhere with this. I did ask on the apcupsd mailing list but the suggestions for how to investigate it were way too technical for my capabilities, and as there appears to be almost no documentation from APC I pretty much gave up.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-04-27 04:45 AM . Last Modified: 2022-05-04 10:16 PM
Hi @Occamsrazor
I can provide you with part of the information here, since we do not support APCUPSD, I am staying away form that part of the conundrum.
For the unit itself, activating Modbus TCP as per the manual should be pretty straight forward.
I did manage to dig up the register map for the units up as well, and you can find it here -> https://www.se.com/us/en/download/document/SPD_LFLG-A32G3L_EN/
As mentioned, how APCUPSD handles modbus TCP, or if it is even supported, is beyond my knowledge, so I will need to pass on that.
But I hope the register map can be a step in the right direction for you.
Best regards
Tonny
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.