Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Search in
Please select a country to continue with beta search.
Free
EnglishStrengthen your foundational knowledge in Data Centers for free, enroll in this path today and start your learning journey!
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 04:41 AM . Last Modified: 2024-03-13 01:32 AM
Hi friends
We just got a new SMART-UPS RT 5000 XL up and running (partially). I am not on site with the device but I have a guy I can coordinate to.
He managed to connect via serial and configure a static IP, subnet, gateway, etc.
However, when I try to connect to the IP in a browser it gives the above error message (seen in attachment too).
Some forums advised to change the home.htm in the address bar to logout.htm but it didn't work (this is for when other users might still be logged in).
He reconnected via serial and opened the SSH port so now I can fiddle around with that, but I am not familiar enough with it to go messing around.
I've also managed to import the device to InfraStruXure manager but it shows up as unknown. When I try to connect to the device via ISX manager it says that someone might already be logged in. (second attachment)
We have also rebooted the device/management card.
Just wondering if anyone is familiar with the error and knows of anything I can try to try and resolve this. This error stops us from getting to the login page so we are unable to configure anything via the webpage.
Thanks in advance.
Daniel
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-11-11 08:48 AM . Last Modified: 2021-11-11 08:49 AM
Hi everybody,
I had the same problem and got around it using PuTTY with the Telnet protocol.
Using the 'web' command here is the result:
apc>web
E000: Success
Http: disabled
Https: disabled
Http Port: 5031
Https Port: 443
Minimum Protocol: TLS1.1
As you can see Web access was disabled.
You can enable it by typing:
web -h enable (for http access) or
web -s enable (for https access)
And you can use web ? for more options.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 04:41 AM . Last Modified: 2024-03-13 01:32 AM
Hi Daniel,
I would suggest try to log into your NMC using an Internet browser using http:// rather than https://
http://XX.XXX.XXX.XX instead of https://XX.XXX.XXX.XX
The image you have attached (protected Object)

Normally means that HTTPS is enabled.
Once you have gained access to your card follow Configuration > network > web > access
Here in the web settings you can enable HTTP
If you cannot gain access, can you log into your card using TelNet?
Kindest Regards,
Richard…
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 04:41 AM . Last Modified: 2024-03-13 01:32 AM
Hey Richard
Thanks for your response!
Ok so I just tried http and unfortunately that doesn't work. I get the same error as before.
I tried to connect via Telnet using putty but got the below message. I get similar errors for Raw and RLogin. SSH seems to let me in though. Can I enable http via SSH?
=================
PuTTY Fatal Error
Network error: Connection refused.
=================
Much appreciated.
Daniel
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 04:41 AM . Last Modified: 2024-03-13 01:32 AM
Whoever set up the card probably disabled insecure protocols like http and telnet. I would try connecting via https:// or reset the card to defaults via SSH.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-06-29 04:41 AM . Last Modified: 2024-03-13 01:32 AM
I checked that with the guy that set it up but he said he wasn't prompted to disable anything. He wouldn't have done so without me saying as he was operating under my instruction in regards to installing and configuring the device. Quite odd. Might give Schneider a call again tomorrow to see if anyone over the phone knows.
Thanks for your help so far everyone.
Daniel
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-11-11 08:48 AM . Last Modified: 2021-11-11 08:49 AM
Hi everybody,
I had the same problem and got around it using PuTTY with the Telnet protocol.
Using the 'web' command here is the result:
apc>web
E000: Success
Http: disabled
Https: disabled
Http Port: 5031
Https Port: 443
Minimum Protocol: TLS1.1
As you can see Web access was disabled.
You can enable it by typing:
web -h enable (for http access) or
web -s enable (for https access)
And you can use web ? for more options.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-02-22 02:16 PM
Works for me, thanks!
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-05-15 04:50 PM
ok its asking to reboot or restart it? how do I do that?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-06-27 05:12 AM
Hi, I'm trying to reenable the HTTP port using a Telnet connectionas unable to connect through web browser after setting to HTTPS and also unable to get the hyperterminal connection to the console port to work.
I've tried a few variations of the 'Web' command but can't get it to work, keep getting 'E102 Parameter Error'.
Can you help me with this?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-07-01 02:22 AM
Sorted this now.
I hadn't noticed that the -S was a capital.
Command to turn on http was:
web -S http
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.