Powerchute Versions and Limitations

APC UPS Data Center & Enterprise Solutions Forum

Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
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
  • Powerchute Versions and Limitations
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
139
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
DBrenner_apc
Crewman DBrenner_apc
Crewman

Posted: ‎2021-06-28 11:35 AM . Last Modified: ‎2024-03-15 04:55 AM

0 Likes
1
858
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
Posted: ‎2021-06-28 11:35 AM . Last Modified: ‎2024-03-15 04:55 AM

Powerchute Versions and Limitations

Hi,

We want to purchase an APC Smart-UPS 3000VA and APC SMC1500IC 1500VA to drive several Servers.
In total these UPS's will be supporting about 3 Windows Server based Server's each. The UPS's will not have
the additional network cards installed. As such:

- Which version of Powerchute will be suitable? Business Edition? Business Deluxe Edition?
- Are all versions of Powerchute free to download and use?

Ideally, is there a comparison chart that let us see the difference's between each version of Powerchute?

Many thanks

Dave

Labels
  • Labels:
  • Smart-UPS & Symmetra LX | RM
  • Tags:
  • PowerChute
  • powerchute_business_edition
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
Administrator

Posted: ‎2021-06-28 11:35 AM . Last Modified: ‎2024-03-15 04:55 AM

0 Likes
0
858
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
Posted: ‎2021-06-28 11:35 AM . Last Modified: ‎2024-03-15 04:55 AM

Hi Dave,

I could probably talk for an hour on the differences between the versions of Powerchute but I'll keep it short, so this is in no way a full list of differences:

Powerchute Personal: Works with APC Back-UPS, Single computer, Windows 7/10 only, USB connection, features kept simple for easy of use, generally for home users

Powerchute Business: Works with Smart-UPS, Single computer/server single UPS, USB or Serial connection, Windows 7/10, Server 2008R2+, some Linux support, advanced features such as the ability to execute scripts, schedule shutdowns, Email and SNMP   

Powerchute Network Shutdown: Works with all UPSs with NMC1/2/3/4, connects over the network, support for large range of O/S, support for virtual and hyper-convened environments, advanced features, supports single or multiple UPS connected to one or more servers  

All versions are free in most countries.

For the setup you have with multiple server and multiple UPS I would recommend looking at adding NMC2/3s to your UPSs to get the most. The other option is to connect one server to the 1500 (for power and by USB) and use PCBE, then connect the other two to the 3000 for power, connect one by USB, install PCBE and create a script to shutdown the other unconnected server during an outage. It's no ideal and creating the script is up to you we don't provide scripts. Also you can really only connect the servers to one UPS or the other whereas if you had network cards you might be able to connect one PSU to one UPS and the second PSU to the other UPS and configure PCNS to make it all work together.

-Gavan 

 

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
BillP
Administrator BillP Administrator
Administrator

Posted: ‎2021-06-28 11:35 AM . Last Modified: ‎2024-03-15 04:55 AM

0 Likes
0
859
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
Posted: ‎2021-06-28 11:35 AM . Last Modified: ‎2024-03-15 04:55 AM

Hi Dave,

I could probably talk for an hour on the differences between the versions of Powerchute but I'll keep it short, so this is in no way a full list of differences:

Powerchute Personal: Works with APC Back-UPS, Single computer, Windows 7/10 only, USB connection, features kept simple for easy of use, generally for home users

Powerchute Business: Works with Smart-UPS, Single computer/server single UPS, USB or Serial connection, Windows 7/10, Server 2008R2+, some Linux support, advanced features such as the ability to execute scripts, schedule shutdowns, Email and SNMP   

Powerchute Network Shutdown: Works with all UPSs with NMC1/2/3/4, connects over the network, support for large range of O/S, support for virtual and hyper-convened environments, advanced features, supports single or multiple UPS connected to one or more servers  

All versions are free in most countries.

For the setup you have with multiple server and multiple UPS I would recommend looking at adding NMC2/3s to your UPSs to get the most. The other option is to connect one server to the 1500 (for power and by USB) and use PCBE, then connect the other two to the 3000 for power, connect one by USB, install PCBE and create a script to shutdown the other unconnected server during an outage. It's no ideal and creating the script is up to you we don't provide scripts. Also you can really only connect the servers to one UPS or the other whereas if you had network cards you might be able to connect one PSU to one UPS and the second PSU to the other UPS and configure PCNS to make it all work together.

-Gavan 
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.