Posted: 2023-06-01 06:14 PM
Back-UPS ES 650 chirps with solid red LED
After the unit started chirping with a solid red LED, I replaced the battery with a new one. 24 hours later the unit began chirping with a solid red LED again. I did not find that specific FAQ. Does this maybe mean the UPS circuitry has failed?
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
Posted: 2023-06-01 08:25 PM
I disconnected all of the devices from the UPS and disconnected the UPS from AC power. After connecting a device to the UPS which was only on battery power, it again started chirping with a solid red LED.
I am now operating the UPS as just a surge protector (all devices are connected to the "Surge Protection Only" side of the UPS). The UPS is connected to AC power. No chirping or lit LED.
Link copied. Please paste this link to share this article on your social media post.