Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Search in
Link copied. Please paste this link to share this article on your social media post.
Hi,
The operation modes are not showing, although I selected the correct object and played around with different colors. Does anybody have an idea?
Thanks in advance.
Regards,
Niels
Posted: 2024-07-22 11:35 AM . Last Modified: 2024-07-22 11:39 AM
Link copied. Please paste this link to share this article on your social media post.
Hello Supersoon,
is this one what you are looking for?
Check the attached projects (ETS + Wiser) and compare the KNX device parameters/Wiser widget settings
with your own project.
Both, KNX device and the widget, are located in to the Living room
Individual address of the MT is 1.1.26
Psw to open the Wiser project is KNXmilan2024
Link copied. Please paste this link to share this article on your social media post.
Hi Supersoon!
Did you linked the dedicated GA's correctly?
Sorry for the german example but this I had just next to me.
But I guess the language is not important here to understand how it works 😉Comparison of Touch Config and ETS
Link copied. Please paste this link to share this article on your social media post.
Hi Thomas,
I did link the correct GA for the operation mode input but there is no operation mode output in the object tab ("Thermostat" widget). I noticed there is something on the bottom left of the widget. When I hoover over it, the arrow turns into a hand symbol. In the "styles" tab, "Mode button color" and "Mode button icon color" do have a color assigned.
The widget is meant to control a Schneider Multitouch pro thermostat. Is this the correct widget to use?
Furthermore I would also like to display the current heating/cooling mode. I've assigned the correct heating/cooling object but I don't see anything on the widget. In the "Styles" tab you can choose which color to use when heating or cooling, but this only works locally on the widget (when the setpoint is higher or lower then the actual temperature). The actual status from the assigned heating/cooling object is not used here. Any idea?
Thanks.
Regards,
Niels
Link copied. Please paste this link to share this article on your social media post.
Thomas,
I just saw in your previous post you used the "Thermostat status alert" to link the operation mode output...
Now I can see the operation mode symbol. However, I can't select another operation mode. How is this possible?
My question regarding the heating/cooling status still remains.
Thanks.
Regards,
Niels
Link copied. Please paste this link to share this article on your social media post.
Hi Supersoon!
Here are some screenshot of how my Multitouch + Touch visu widget is configured.
I hope it helps to solve your issue
Clicking on the Operation mode icon, a 2nd window is opening from which you can select the desidered mode
Link copied. Please paste this link to share this article on your social media post.
Hi Supersoon,
it could be helpfull to know which kind of controller you are using.
Can you share that information with us?
Link copied. Please paste this link to share this article on your social media post.
Hi,
Thanks everybody for the assistance so far ;-). I've got the operation modes showing 👍
The thermostat is a Multitouch Pro System Design to control the floor heating/cooling.
As you can see in the attached screenshots I've assigned the widgets "heating/cooling status" object and set the heating color to "red" and cooling to "blue" but I can't see the color of the actual temp changing.
When I switch the object manually between "0" cooling and "1" heating it keeps having the blue color.
Also the 'Is active" object is not showing when there is a request for heating or cooling.
Thanks in advance,
Regards,
Niels
Posted: 2024-07-22 11:35 AM . Last Modified: 2024-07-22 11:39 AM
Link copied. Please paste this link to share this article on your social media post.
Hello Supersoon,
is this one what you are looking for?
Check the attached projects (ETS + Wiser) and compare the KNX device parameters/Wiser widget settings
with your own project.
Both, KNX device and the widget, are located in to the Living room
Individual address of the MT is 1.1.26
Psw to open the Wiser project is KNXmilan2024
Link copied. Please paste this link to share this article on your social media post.
Hi Cristiano,
Thanks, I will create separate widgets to reflect the heating/cooling mode.
As a feature request I would like to see the mode in the thermostat object itself.
Kind regards,
Niels
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.