SpaceLogic KNX Hybrid Module vs RGB
Hi,
LSS100400:
I dont understand how to control the RGB lights from a zigbee device.?
There is only conventional dimmer group adress possibillities??
(It`s working through HUE gatway and a script. (it`s to unstable)
and the point with the Hybrid module is to get rid of all the other gatways)
BR
GIA
- Labels:
-
Wiser for KNX
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
okay, I see that this LS100400 only support ELKO++ ;(
--> But Elko does not have RGB dimmers! Is there a workaround by using script through LS100400?
BR
GIA
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
Hello GIA!
Sorry, but it is not fully clear to me what you are looking for.
One hand you wrote to "how to control the RGB lights from a zigbee device" which means for me, you have a Zigbee Controller or Pushbutton which you want to use to control a RGB-Light within KNX.
On the other hand I guess you try to link a non SE RGB-Lights (Zigbee) with our Hybrid Module to control it from the KNX-World?
Thomas
Application Design Engineer
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
Some devices like GLEDOPTO e27 Lights can be controlled with the library:
When device is inserted, it doesn't have any R,G,B, W or Colour Temperature Variable to get controled, but using the library (direct zigbee command) it is possible.
or color temperature:
You can try to use library to control this device.
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
Hi Thomas,
yes I want to use the hybrid module to control zigbee RGB dimmer devices (non SE RGB-Lights (Zigbee) actuators). I have both KNX and zigbee pushbuttons.
Perhaps the soulution Esteve mention, that there is some possibilitis in a library that I should explore.
BR
GIA
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
Tanx for the reply 🙂
I will try to explore this function.
BR
GIA