SpaceLogic KNX Forum
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Link copied. Please paste this link to share this article on your social media post.
Hi,
i am fairly new to the whole knx world and hope you can help me.
I plan on using several of the Spacelogic Minis in my house. Beside switching and setting parameteres I really would like them to show if a window is open or if there is a fault somewhere. So far I have not found anything that I can use for this purpose. In my understanding something like the "weather information" toggle sun/rain would be great if I could use it independent with different icons.
Hope somebody can help me on this as it is a huge deal breaker at the moment.
thank you for any support,
regards,
Robert
Link copied. Please paste this link to share this article on your social media post.
Hi Robert!
Welcome to this forum and to KNX in general 😊
Nice to hear that you like the 4" MiniTouch!
Regarding your topic, I fully agree with you that we should have such kind of functionality.
Two parts:
1. Window/door contact
You could use, as a kind of workaround, to use the switching function.
But in this case, when you click on the icon you will change the status while the window is untouched.
So it would show a wrong status only until a new cyclic telegram (from the window sensor) will arrive.
When nobody touches the icon, it will represent the status of the window correctly.
2. The fault visualization could work in the same way, but you would need to upload a dedicated customized icon as it is not part of the delivered set of default icons.
Link copied. Please paste this link to share this article on your social media post.
Hi Thomas,
thank you very much for your create solution this is very appreciated.
Do you see a chance to get a „status function“ properly included in one of the next firmware updates?
I am not too sure how the other household members are able to cope with a switchable status 😉
Regards,
Robert
Link copied. Please paste this link to share this article on your social media post.
Hi Robert!
to "Do you see a chance to get a „status function“ properly included in one of the next firmware updates?"
I will double check if this feature request is not already noted. If not, I will place it.
to "I am not too sure how the other household members are able to cope with a switchable status "
I think it is pretty clear for all that you cant open a pure mechancial window without having a dedicated motor.
Means when you press it ... nothing will happen.
In case you make the cycletime somehow arround 10s or less then the status will be updated pretty soon.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.