SpaceLogic KNX Forum
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Link copied. Please paste this link to share this article on your social media post.
hello Dears,
I used the Built in Thermostat widget, In touch it has an on/off Icon and working well, but in the Wiser for KNX Mobile App it didn't appear.
Currently, I’m using a separate on/off function, but it would be ideal to have the on/off feature integrated within the thermostat itself. Is this normal, or should it be visible in the app’s thermostat widget? If so, how can I make it appear there?
Link copied. Please paste this link to share this article on your social media post.
Hi
Also in the next release (end of Sept/Beginning of October) this should be fixed and now the Thermostat should be able to show the on/off button in the App too. This week the team should test all functionality so we can start field test right after. And then release it to production.
Thanks
Fernando
Link copied. Please paste this link to share this article on your social media post.
Hello IC-Systems,
Many THANKS for the hint. I forwarded your topic to our R&D.
Link copied. Please paste this link to share this article on your social media post.
Thank you @Thomas_Rohde
I attempted to create a custom widget for use in the Wiser app but was unfortunately unsuccessful. If it is possible to create a custom widget for the mobile app, I would appreciate it if you could share the process.
Link copied. Please paste this link to share this article on your social media post.
Hi
Also in the next release (end of Sept/Beginning of October) this should be fixed and now the Thermostat should be able to show the on/off button in the App too. This week the team should test all functionality so we can start field test right after. And then release it to production.
Thanks
Fernando
Link copied. Please paste this link to share this article on your social media post.
Hello Dears,
could you please add more options to the setpoint step.
I have a project where the setpoint step is 1 °C not 0.1 nor 0.5
while this will make some conflict in the control.
Link copied. Please paste this link to share this article on your social media post.
Hi,
Did the update already release with this function?
Thanks
Luis Silva
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.