Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Search in
Link copied. Please paste this link to share this article on your social media post.
Hi,
I seem to be unable to activate the long press for a switch on my Spacelogic TouchUnit.
The manual says I should activate the "multiple operation" switch and this should give me options for short/long press and release.
When I select "multiple operation" there are only options for four outputs that can do different things. There no options for long/short etc.
Yes, the long press time in general is set (it is also impossible to not set it).
Has anybody an idea how to solve this?
Thank you,
regards,
Robert
Link copied. Please paste this link to share this article on your social media post.
I don't think there is an "edge" function available at the moment (just checked), only solution i see is to use a scene output button with long press enabled an use a logic block to convert for example value = 0 to 1 bit OFF and value = 128 (long press output) to 1 bit ON...
Link copied. Please paste this link to share this article on your social media post.
Hi,
thank you for your reply and your suggested work around.
I was specifically referring to the options described in the manual und "multiple operations".
There seem to be no long/short press options in my menu?
Link copied. Please paste this link to share this article on your social media post.
Hello Robert_W!
You are fully right! There is something written in the manual what is in real life not there.
It seems it was included accidently.
But it general the 4" is capable to support a long press functionality within some function like Dimm/Blind/Scene but NOT as a kind of Edge-Function which you may know from other of our pushbutton.
You can use of course the workaround proposed by Erwin ... please have in mind that the parameter "Long operation for screen after" is for the whole device! Means if you adapt it, to realize a workaround for edge function, it influences also the long press time for the other configured functions like Dimming, Shutter/Blind etc..
Link copied. Please paste this link to share this article on your social media post.
Are there any plans to update the software on these devices? The product seems unpolished and unfinished in its current state. In addition to the case Robert_W is pointing out here there also seems to be other lacking features, labels are not centered, touch input is way to sensitive (if you try to swipe to a screen you will accidentally press a button or function). All in all I am little disappointed as the discontinued touch panels were pretty good as they were. My expectation is that a new product should be a little bit better than the product it replaces - I don't feel this product ticks that box.
Link copied. Please paste this link to share this article on your social media post.
Hello Ratorg!
Many THANKS for your constructive feedback.
It will help to improve our products within upcoming releases.
I will forward your feedback to the dedicated offer manager.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.