KNX dimmer: MTN649325 4 channels and MTN649310 1 and 12V PHILIPS LED MR16 LV 10W
SpaceLogic KNX Forum
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
The Power adapter is 127 V and MTN649325 works with 220 V... even adjusting mximum to 50% regulation.. who can be sure that 100% voltage from KNX actuator is not applied to Tansformer lamps?
Link copied. Please paste this link to share this article on your social media post.
2015-01-2803:50 AM
Hello Sabrina! Probably yes! It looks like the one we use in our KNX training kit. However, as mentioned by @esteve budia, the power adapter installed is a 220V one. Tomorrow, I'll be at SE and we can have a look on that.