KNX dimmer: MTN649325 4 channels and MTN649310 1 and 12V PHILIPS LED MR16 LV 10W
Are the KNX dimmer: MTN649325 4 channels and MTN649310 1 channel compatible with 12V PHILIPS LED MR16 LV 10W, power supply PHILIPS ET-R-50A16?
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
Maybe dimmer-test guys .. Sabrina.
http://schneider-electric.dimmer-test.com/
The Power adapter is 127 V and MTN649325 works with 220 V... even adjusting mximum to 50% regulation.. who can be sure that 100% voltage from KNX actuator is not applied to Tansformer lamps?
In my opinion no way
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
Hello Sabrina! Probably yes! It looks like the one we use in our KNX training kit. However, as mentioned by @esteve budia, the power adapter installed is a 220V one. Tomorrow, I'll be at SE and we can have a look on that.