Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

KNX Multitouch Pro temperature measurement

SpaceLogic KNX Forum

Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
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
  • EcoStruxure Building
  • Light and Room Control
  • SpaceLogic KNX Forum
  • KNX Multitouch Pro temperature measurement
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Thomas_Rohde
Sisko Thomas_Rohde Sisko
132
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
60
Heribert_Dölger
Commander Heribert_Dölger Commander
31
View All

Recommended Forums

  • Intelligent Devices Forum

  • SmartConnector Forum

  • Metering & Power Quality

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to SpaceLogic KNX Forum
Start a Topic
Solved
IC_Systems
Captain IC_Systems
Captain

Posted: ‎2024-08-22 07:22 AM . Last Modified: ‎2024-08-22 07:24 AM

0 Likes
2
903
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
‎2024-08-22 07:22 AM

KNX Multitouch Pro temperature measurement

Hello dears,

I have observed that the internal temperature reading of the Multitouch Pro (MTN6215-5910) is inaccurate when mounted inside its wall box. However, the reading becomes more accurate when the device is removed from the mounting box.

I did not use any external temperature sensor, relying solely on the internal sensor for temperature measurement.

is there a default value for the internal sensor correcting facture that I should use?

Please refer to the attached pictures for further details.

WhatsApp Image 2024-08-22 at 17.20.48_cb9567b1.jpg

 

WhatsApp Image 2024-08-22 at 17.20.48_87e73a22.jpg

 Both York and MT is showing the ambient temperature

Best Regards,
Labels
  • Labels:
  • SpaceLogic devices
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Thomas_Rohde
Sisko Thomas_Rohde Sisko
Sisko

Posted: ‎2024-08-28 12:57 AM

1 Like
0
828
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
‎2024-08-28 12:57 AM

Hello IC_Systems!

The topic is a bit tricky as it can be influenced by several topics.
First one is of course is the one Esteve mentioned above.
Another topic can be the wall itself where the product is installed in.
Means, if the wall on the other side has a big temperature difference ... it can influence the temperature measurement in one or the other way.
Another topic is airflow. Depending on the installation place, there can be a bigger airflow, in case the next room has a much different temperature.
Another topic is sunlight. Our product is pretty dark and heats up more quickly as a white one.

Another topic is the time of measurement. It seems your device on top is not using any design frame.
Means, I guess, the airflow can go easily through the device and can react pretty quickly on temperature changes. Our product has no direct openings and is installed within a designframe. This leads to the consequence that our device does not react so quickly on temperature changes.
This gives also the answer for the picture where our device is outside the wall => it measures more accurately and quickly the correct temperature.
Taking all topics from above into consideration, it makes it clear that, there is no "standard correcting value" available. It is always pretty depending on the place of installation and the surrounding environment.

 

Kind regards
Thomas

Application Design Engineer

See Answer In Context

Reply
Replies 2
esteve_budia
Lieutenant esteve_budia Lieutenant
Lieutenant

Posted: ‎2024-08-26 11:36 PM

1 Like
0
847
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
‎2024-08-26 11:36 PM

Sometimes it is a problem with the tube that carries the cables, through which air currents are produced. Have you been able to try sealing the pipeline (with a sealant or a simple paper for testing) ?

Reply
Thomas_Rohde
Sisko Thomas_Rohde Sisko
Sisko

Posted: ‎2024-08-28 12:57 AM

1 Like
0
829
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
‎2024-08-28 12:57 AM

Hello IC_Systems!

The topic is a bit tricky as it can be influenced by several topics.
First one is of course is the one Esteve mentioned above.
Another topic can be the wall itself where the product is installed in.
Means, if the wall on the other side has a big temperature difference ... it can influence the temperature measurement in one or the other way.
Another topic is airflow. Depending on the installation place, there can be a bigger airflow, in case the next room has a much different temperature.
Another topic is sunlight. Our product is pretty dark and heats up more quickly as a white one.

Another topic is the time of measurement. It seems your device on top is not using any design frame.
Means, I guess, the airflow can go easily through the device and can react pretty quickly on temperature changes. Our product has no direct openings and is installed within a designframe. This leads to the consequence that our device does not react so quickly on temperature changes.
This gives also the answer for the picture where our device is outside the wall => it measures more accurately and quickly the correct temperature.
Taking all topics from above into consideration, it makes it clear that, there is no "standard correcting value" available. It is always pretty depending on the place of installation and the surrounding environment.

 

Kind regards
Thomas

Application Design Engineer
Reply
Preview Exit Preview

never-displayed

You must be signed in to add attachments

never-displayed
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.