Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

KNX/DALI gateway - Philips Xtanium

SpaceLogic KNX Forum

Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
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
  • EcoStruxure Building
  • Light and Room Control
  • SpaceLogic KNX Forum
  • KNX/DALI gateway - Philips Xtanium
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Thomas_Rohde
Sisko Thomas_Rohde Sisko
132
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
60
Heribert_Dölger
Commander Heribert_Dölger Commander
31
View All

Recommended Forums

  • Intelligent Devices Forum

  • SmartConnector Forum

  • Metering & Power Quality

Related Products
product field
SpaceLogic KNX - 4ʺ Touch Unit
product field
KNX Push Button Dynamic Labeling, universal
product field
Wiser for KNX : logic controller

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to SpaceLogic KNX Forum
Start a Topic
sesa174915
sesa174915 Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2015-01-28 01:00 AM . Last Modified: ‎2024-07-15 12:03 AM

1 Like
5
1070
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
‎2015-01-28 01:00 AM

KNX/DALI gateway - Philips Xtanium

We have some issues with the KNX/DALI gw MTN6725-0001 firmware 1.2.0 in combination with Philips Xtanium LED panels. Control works fine for a while (sometimes weeks) but then dimming stops working. Also we can no longer connect via ETS plug-in to the DALI gw. When we reload the application or cut the power, everything works fine again. Any suggestions ? Does anyone have experience with a DALI analyser ? In attachment you can find the datasheet for the LED panel.

  • Thumbnail of SpaceLogic KNX - 4ʺ Touch Unit
    SpaceLogic KNX - 4ʺ Touch Unit
  • Thumbnail of KNX Push Button Dynamic Labeling, universal
    KNX Push Button Dynamic Labeling, universal
  • Thumbnail of Wiser for KNX : logic controller
    Wiser for KNX : logic controller
View products (3)
Attachments
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 5
esteve_budia
Lieutenant esteve_budia Lieutenant
Lieutenant

Posted: ‎2015-01-28 01:00 PM

0 Likes
0
989
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
‎2015-01-28 01:00 PM

Reply
Heribert_Dölger
Commander Heribert_Dölger Commander
Commander

Posted: ‎2015-02-04 02:36 AM

0 Likes
3
989
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
‎2015-02-04 02:36 AM

Hello Hannes

We had some problems with Philips Xitanium ballasts in the past. These problems were related to addressing the LED drivers. Once they received a DALI short address it was not possible to modify this address. Philips is expecting a special procedure for doing this (which BTW is not according to DALI standard).

Nevertheless we modified the firmware of the KNX DALI Gateway and this is now supported. This installation contains several thousand of these Philips Xitanium LED drivers (but is different type that used in your project). The installation is working properly now for several months.

Two times we saw thermal problems of ballasts (from different manufacturers) that were mounted in a false ceiling without ventilation. Ballasts could not be controlled. Only after reset of the ballasts the installation worked again.

Are you resetting the KNX DALI Gateway only? Or do you have as well to reset the ballasts? You mentioned that after download of the application everything works fine. I wonder that before you couldn't communicate with ETS but it seems you are able to download the application. Do I understand correctly that only donwnload of application (without resetting KNX DALI Gateway or LED drivers) makes it work again?

BR, Heribert

Reply
sesa174915
sesa174915 Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2015-02-04 04:41 AM

0 Likes
2
989
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
‎2015-02-04 04:41 AM

Hello Heribert,

The integrator suspects that when he did the application download, the installer powered down/up the DALI gateway before he arrived.

So, sometimes only powering down/up the DALI gateway solves the problem. Other times you also need to download the application.

The ballasts remain powered. By resetting the DALI ballasts you mean cutting the power to the ballasts ?

Downloading the application works but when we open the plug-in we can't connect to the DALI gateway.

It has been weeks since the last problem, but this was the case the last time aswell.

Kind regards,

Hannes

Reply
Heribert_Dölger
Commander Heribert_Dölger Commander
Commander

Posted: ‎2015-02-04 08:06 AM

0 Likes
0
989
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
‎2015-02-04 08:06 AM

Hello Hannes

I would propose to check the following.

When the error occurs

- is there the possibility to control the lamps by the use of the buttons on the device
- is it possible to connect to the DALI Gateway via IP connection (web interface) and control the lamps
- is the display reacting on commands initiated by the buttons on the device?

This of this is to find out if there is still communication from the device to the DALI line but no communication from KNX bus.

Some more questions:

When was the firmware update done?

Are you sure that you are using firmware 1.2.0? It was released in November last year. As you mention the installation works well for weeks I guess the update was done not that long ago. Please doublecheck if really the latest firmware is on the device. Version number is indicated on the display.

Do you know how old the devices are?

Are the DALI gateways integrated in an IP network?

Best regards
Heribert

Reply
Heribert_Dölger
Commander Heribert_Dölger Commander
Commander

Posted: ‎2015-02-05 03:53 AM

0 Likes
0
989
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
‎2015-02-05 03:53 AM

Hello Hannes

some more ideas what could cause your problem:

The DALI Gateway has several modes that cause that the lamps can no longer be controlled:
- panic mode
- test of emergency lamps
- burn-in of new lamps

Please check if one if these modes is active when you see the problem that lamps can no longer be controlled.

BR
Heribert
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.