Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

KNX DALI-Gateway Basic REG-K - Firmware update

SpaceLogic KNX Forum

Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
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
  • EcoStruxure Building
  • Light and Room Control
  • SpaceLogic KNX Forum
  • KNX DALI-Gateway Basic REG-K - Firmware update
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Thomas_Rohde
Sisko Thomas_Rohde Sisko
132
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
60
Heribert_Dölger
Commander Heribert_Dölger Commander
31
View All

Recommended Forums

  • Intelligent Devices Forum

  • SmartConnector Forum

  • Metering & Power Quality

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to SpaceLogic KNX Forum
Start a Topic
Solved
PiotrJakubczyk
Sisko PiotrJakubczyk Sisko
Sisko

Posted: ‎2025-05-15 11:58 PM . Last Modified: ‎2025-05-16 12:10 AM

0 Likes
1
608
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
‎2025-05-15 11:58 PM

KNX DALI-Gateway Basic REG-K - Firmware update

 

I'm reading "Special Instructions for Update from 0.2.x to 0.3.x and downgrade" provided with 

"MTN6725-0004 DALI-Gateway Basic REG-K Firmware 0.3.5 for ETS Application 7313 (0.3.5)" 
 

https://www.se.com/il/en/product/MTN6725-0004/knx-daligateway-basic-regk-2-16-64/

 

Special Instructions for Update from 0.2.x to 0.3.x and downgrade
Please note that with firmware 0.3.0 an extensive expansion of the device's function has been carried out. This firmware re-quires the ETS applications 7312/1.1 for MTN6725-0003 and 7313/1.1 for MTN6725-0004 and the corresponding DCA SpaceLogic KNX DALI Gateway Basic Plus V1.1.2.0. Commissioning with the old application and old DCA is not possible. If a device with firmware 0.3.x is to be loaded with the old application (e.g. when replacing a device or expanding an existing installation), it must first be downgraded to 0.2.7. A special downgrade file is available for this purpose: "Firmware 0.2.7 Downgrade". When downgrading, any existing data in the unit will be deleted (physical address, etc.).
When updating from version 0.2.x to 0.3.0, all data is also deleted. The device must then be reloaded with the ETS and the DALI data must be restored with the restore function in the DCA (see also the description of the application program). Please note that the unit is initially loaded with firmware 0.3.0 or 0.3.1. Firmware versions higher than 0.3.1 must not be loaded directly into units with 0.2.x, as these are not "Unconditional". In this case, the update must be carried out in two steps. First to 0.3.1, then in a second step to e.g. version 0.3.2.

 

There are references to "Firmware 0.2.7 Downgrade" but no such firmware provided in pack. Is this instruction is obsolete? What i should do with "MTN6725-0004_Firmware_Upgrade_to_V0_3_0" and what "MTN6725-0004_Firmware_Update_0_3_5.zip"

 

I should replace "Firmware 0.2.7 Downgrade" with "MTN6725-0004_Firmware_Upgrade_to_V0_3_0" ?

 

PiotrJakubczyk_0-1747378788045.png

 

 

"Please note that with firmware 0.3.0 an extensive expansion of the device's function has been carried out" Noted this on front of device with black marker but still don't know how to upgrade 🤔. Someone can translate from R&D to English? 😁

Labels
  • Labels:
  • SpaceLogic devices
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Thomas_Rohde
Sisko Thomas_Rohde Sisko
Sisko

Posted: ‎2025-05-23 01:37 AM . Last Modified: ‎2025-05-23 01:37 AM

1 Like
0
557
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
‎2025-05-23 01:37 AM

Hello Piotr!

It says that you should be carefull with the update in the way that it requires a new ETS-Applicaton with the dedicated DCA.

Means => In case you have an existing ETS configured running device and you want to perform this update (because you are interested in the new features) ...
You need to use a different (new) DCA and ETS-Application as you used before.

 

Kind regards
Thomas

Application Design Engineer

See Answer In Context

Reply
Reply 1
Thomas_Rohde
Sisko Thomas_Rohde Sisko
Sisko

Posted: ‎2025-05-23 01:37 AM . Last Modified: ‎2025-05-23 01:37 AM

1 Like
0
558
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
‎2025-05-23 01:37 AM

Hello Piotr!

It says that you should be carefull with the update in the way that it requires a new ETS-Applicaton with the dedicated DCA.

Means => In case you have an existing ETS configured running device and you want to perform this update (because you are interested in the new features) ...
You need to use a different (new) DCA and ETS-Application as you used before.

 

Kind regards
Thomas

Application Design Engineer
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.