Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

IP Tunneling setting help needed

SpaceLogic KNX Forum

Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
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
  • EcoStruxure Building
  • Light and Room Control
  • SpaceLogic KNX Forum
  • IP Tunneling setting help needed
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Thomas_Rohde
Sisko Thomas_Rohde Sisko
132
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
60
Heribert_Dölger
Commander Heribert_Dölger Commander
31
View All

Recommended Forums

  • Intelligent Devices Forum

  • SmartConnector Forum

  • Metering & Power Quality

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to SpaceLogic KNX Forum
Start a Topic
Solved
miklosbakos
Crewman miklosbakos
Crewman

Posted: ‎2024-08-22 03:20 AM

0 Likes
10
4462
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
‎2024-08-22 03:20 AM

IP Tunneling setting help needed

Hi Team, That's a super beginner question I need help with. Previously the LSS100100 worked well, I was able to program individual devices on the KNX network, and the LSS100100 listened to the network traffic and update GA values, so everything was fine.
Now, I'm not able to even download the application in ETS sw. The settings and issues explained below:

LSS100100 KNX network settings (please find screenshot):

Mode=IP Tunneling

Tunneling router IP: the IP of the LSS100100

KNX address is set

Enabled IP routing, Enabled passed individual telegrams, and accepted IP Tunneling.

Topology: there are 15 devices on KNX simple line network (red/black wires), plus the LSS100100 connected, my PC and LSS100100 are connected through a wifi router.

With the above settings, the ETS software cannot discover the device, so I added manually, Test=OK. However, when I try to download an app to a previously programmed device (blind control) it gave an error message saying "The current subnetwork of the interface does not exist in your project. Do you want to change your local settings now? Interface: New Connection - 192.168.1.162:3671(15.15.100)", I accept the changes but it brings back the Individual address panel to set it up, and it just in this loop, error/change the local setting/ask for induvidual address/starts again...

I know this settings is very basic, but I spent hours on this, I tried a bunch of different things, but now I don't have more options...

There is a KNX/IP interface device (MTN6502-0105) on the Network as well (disconnected from the router now), with that device the ETS software works fine.

Can you please help me with the right KNX network settings of the LSS100100?

Thank you

 

BR

Miklos

Attachments
Labels
  • Labels:
  • Wiser for KNX
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Cristiano_Carli_Ballola
Lt. Commander Cristiano_Carli_Ballola Lt. Commander
Lt. Commander

Posted: ‎2024-08-24 12:29 AM

1 Like
1
4389
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
‎2024-08-24 12:29 AM

Two main issues on your LSS100100 configuration:

  1. as already mentioned by @Erwin-vd-Zwart , if your Wiser for KNX controller is connected to the bus via the KNX cable, the KNX connection has to be set as TP-UART
  2. The individual address of the controller must match the topology:
    you probably do not have an area 15 and a line 15 in your system.
    Therefore, change the individual address so that it indicates its actual position in your project.
    This is also the reason for the ETS error message.

See Answer In Context

Reply
Replies 10
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
Janeway

Posted: ‎2024-08-22 09:04 PM . Last Modified: ‎2024-08-23 02:10 AM

0 Likes
3
4426
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
‎2024-08-22 09:04 PM

Why is the device in tunnel mode?

 

Just set it to TPUART and make sure KNX IP Routing is enabled, then it will work like your other IP interface

Reply
miklosbakos
Crewman miklosbakos
Crewman

Posted: ‎2024-08-24 12:05 AM

0 Likes
2
4357
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
‎2024-08-24 12:05 AM

Thank you for your reply.

I’ve tested it earlier but there is an error: no TPUART connection, would you like to switch to KNXIP instead?

By the way, there are 3 settings below TPUART that’s related to KNXIP, should I enable all?

The bus and the installed devices work well, the LSS100100 is installed in the middle of the bus, so the physical connection has to be right.

Any idea how can I do some debug to find the issue? Or any other way I can connect the LSS100100 to the KNX bus?

Thank you

BR

Miklos

Reply
Cristiano_Carli_Ballola
Lt. Commander Cristiano_Carli_Ballola Lt. Commander
Lt. Commander

Posted: ‎2024-08-24 12:29 AM

1 Like
1
4390
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
‎2024-08-24 12:29 AM

Two main issues on your LSS100100 configuration:

  1. as already mentioned by @Erwin-vd-Zwart , if your Wiser for KNX controller is connected to the bus via the KNX cable, the KNX connection has to be set as TP-UART
  2. The individual address of the controller must match the topology:
    you probably do not have an area 15 and a line 15 in your system.
    Therefore, change the individual address so that it indicates its actual position in your project.
    This is also the reason for the ETS error message.
Reply
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
Janeway

Posted: ‎2024-08-26 09:13 PM

0 Likes
1
4351
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
‎2024-08-26 09:13 PM

Can you try replace the red/grey KNX connector with another one, if your bus is powered, working and connected to the Wiser then you should not have the error on TPUART so either you have a bad TP connection or the device is malfunctioning, probably the first…

Reply
miklosbakos
Crewman miklosbakos
Crewman

Posted: ‎2024-08-30 05:27 AM

0 Likes
0
4311
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
‎2024-08-30 05:27 AM

Thank you for both.

Unfortunately, I've already tried the TPUART, but either ETS says no connection with the KNX device when I try to download, OR the LSS100100 shows an error message: "KNX/TP is not connected. Scripting, visualization and other features may not work. DO you want to switch to KNX/IP instead?". So it seems the LSS100100 doesn't communicate with the TPUART network at all. Wire connections are fine.

So the only solution I have is to try to establish the connection through KNX/IP routing (or maybe tunneling). I would buy a new device only if it is really necessary.

Is there any way I can communicate with KNX devices on the TPUART network with utilising the LSS100100 and the working KNX/IP device?

Any advice is appreciated.

Thank you

Miklos

Reply
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
Janeway

Posted: ‎2024-08-30 10:26 PM . Last Modified: ‎2024-08-30 10:27 PM

0 Likes
2
4271
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
‎2024-08-30 10:26 PM

If you have devices and PSU connected to the TP of the controller and you get the TP disconnected message you either need to check the connection and check 30V , also check when you have a PSU with secondary power output that you have connected the BUS otherwise the choke is missing (i have seen this more often), if all of this still give you the message on TPUART your device is probably damaged ..

Reply
miklosbakos
Crewman miklosbakos
Crewman

Posted: ‎2024-08-31 11:07 PM

0 Likes
0
4233
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
‎2024-08-31 11:07 PM

Yes I swap the terminals of LSS100100 and the well-operating KNXIP Gateway, the result is the same, I can communicate through the KNXIP properly but not with LSS100100. Yes I said it is a hardware issue. Is there any settings I can utilise the LSS100100 with the KNXIP gateway to get a solution for this hardware issue? Or the only solution is to buy another device?

Reply
miklosbakos
Crewman miklosbakos
Crewman

Posted: ‎2024-09-01 10:50 PM

0 Likes
1
4235
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
‎2024-09-01 10:50 PM

Thank you all for your helpful replies.

The device is damaged.

So the final solution is that I set up the KNXIP gateway as the IP Tunneling router, please have a look at the screenshot attached.

 

BR

Miklos

Attachments
Reply
DCD110
DCD110
Cadet

Posted: ‎2025-01-22 10:54 AM

0 Likes
0
3427
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
‎2025-01-22 10:54 AM

Dear community,

 

since today I have exactly the same issue. My traffic lights have been in red with 520% total percentage of controller total utilization. So I followed this guide and enabled ACK in all telegroups.

 

This has solved the traffic light issue. But now I have no more control over my Wiser for KNX device. I cannot access it remote. I've been trying to fix it for hours now, unfortunately without success.

 

Can someone please tell me what I need to do? Thank you!!

  • Thumbnail of Wiser for KNX : logic controller
    Wiser for KNX : logic controller
View products (1)
Tags (2)
  • Tags:
  • Remote access error
  • wiser for knx
Reply
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
Janeway

Posted: ‎2025-01-22 09:59 PM

0 Likes
0
3412
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
‎2025-01-22 09:59 PM

@DCD110 Does it work normal when locsl? You mentioned that the traffic light issue is solved, i assume you can still access the controller to determine that..

 

How do you approach the controller remotely? Via VPN or port forwarding, do you approach it with ETS or via a web browser?

 

in other words can you give more details in the problem you are facing as changing the ACK setting normally can’t result in your issue in any way..
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.