Posted: 2017-10-23 10:43 AM . Last Modified: 2024-07-14 11:51 PM
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
FW 2.1.0 homeLYnk sends only off
Hi.
I have to homeLynk´s, Master with fw 2.1.0 and the Slave has fw 2.0.1.
There is 2 U.motion 10'' slave panels connected to the Master.
I can only turn the lightning off if the telegram is 1bit from slave panels and from
visu button in HL. See Pic,1
I have also tried to clear the browsing data after the fw update.
Pic,1
But i can turn it on / off inside the configurator.
It is also working from the slave visu button with fw 2.0.1.
I recorded the telegrams for Downlights Lobby 101 when i tried to turn the lights on. Sends only Off.
I will attach backup from Master and Salve HL.
BR
Martin Rausch
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
Hello Martin,
We've just released update package which should solve your problem. We've found this bug friday last week and today we've been verifying this update package.
Update package for Wiser for KNX and spaceLYnk fw 2.1.0
Let us know if your problem was solved.
- Solutions team
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
Thank you Petr for the update.
BR
Martin Rausch
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
Hi Petr.
The update package worked realy great, No problem any more.
BR
Martin Rausch