Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric SpaceLogic KNX forum to get support and share knowledge including selection, installation and troubleshooting for spaceLYnk, Wiser for KNX, eConfigure KNX, SpaceLogic KNX Hybrid module and other topics.
Search in
Link copied. Please paste this link to share this article on your social media post.
Hello
Let's start with this quite annoying bug with the ? instead of °C can't find anyway to change it so I guess it's in the firmware
Next
Is there anyway to get rid of the ON/OFF button? I just want to adjust the temperature and tired just about any controller and can't find anyone without it.
Also, the internal temperature sensor is waaaay off. Correct temperature is around 21°C, is this fixable somehow, it also seams to react and rasing multiple degrees just by waking up the screen.
Last, I can't find away to disable settings menu or make it hidden/lock it, is it possible somehow?
(ps please bring back the mtn6215-0310, so much more userfriendlier)
Link copied. Please paste this link to share this article on your social media post.
1)
https://community.se.com/t5/SpaceLogic-KNX-Forum/MTN6215-0410-firmware-upgrade/m-p/477309
did you adapted the ETS-Project-Setting accordingly?
Link copied. Please paste this link to share this article on your social media post.
Hello Jonass!
To "Let's start with this quite annoying bug with the ? instead of °C ...."
Piotr is right to point to the ETS-Setting.
To "Is there anyway to get rid of the ON/OFF button?"
Currently directly within the ETS ... NO. You are right this is not perfect and so it will be changed with the next FW-Update. In case you can realize a certain logic, very simple to realize when there is also a W4K (LSS100100) already in the project, that in case someone pressed this button the GA is directly switched ON again. This would be the workaround to solve the isse immediately.
To "Last, I can't find away to disable settings menu or make it hidden/lock it, is it possible somehow?"
NO, not yet. We got this feedback already and we have reacted on this as it will be part within the next FW-Update.
But many THANKS for your honest and constructive feedback!
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
The first was me being stupid and not seeing the big blue screen notification with utf-8 🫣
Nice if there will be a firmware update later, just have to find away to convince customer that it's a display diming for now. More difficult with the settings but have to come up with something.
If only there also would be a soulution for the temperature sensor also.
Link copied. Please paste this link to share this article on your social media post.
Found another thing. MTN6215-0310 sent Setpoint when there was a input on Current Setpoint Status, this one dosen't 😥. Is this possible to fix? (or maybe just bring back the old panel 🫣)
Link copied. Please paste this link to share this article on your social media post.
Can you elaborate on this? As i read this as following:
Multi Touch Pro sends his current setpoint when there is an update received on the setpoint status object. The 4” doesn’t do this..
Is that not the other way around?
Can't image the setpoint is send from the device when the setpoint status object is written..
Normal behavior would be that the setpoint status is send when the user changes the setpoint or when the setpoint object receives a new value (setpoint is changed on the device and new setpoint status is send)
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.