VFD WIRING HELP

Solutions for Motor Management

Get support to configure, troubleshoot, update or upgrade your motor management solution built with Altivar variable speed drives and Tesys devices to start, control, protect and monitor Low Voltage and Medium Voltage motors and loads, covering direct start, soft start and variable speed control.
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
  • Industrial Automation
  • Solutions for Motor Management
  • VFD WIRING HELP
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
BJacqz
Commander BJacqz Commander
49
LeoLazzaro
Lieutenant LeoLazzaro Lieutenant
16
PriscilaCunha22
Lieutenant JG PriscilaCunha22 Lieutenant JG
15
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Solutions for Motor Management
Start a Topic
Solved
kishore1march
Lieutenant JG kishore1march
Lieutenant JG

Posted: ‎2022-06-01 02:50 AM

0 Likes
2
2816
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
Posted: ‎2022-06-01 02:50 AM

VFD WIRING HELP

Dear,

 

SITE CONDITION - I have a panel with a VFD 90KW and a same capacity of soft starter, where a 75 sqmm cable is being connected to L1,L2,L3 terminals of VFD and another three cables of same size is being looped from VFD input terminals to soft starter input terminals(L1,L2,L3). Now the VFD and Soft starter L1,L2,L3 are looped without any individual MCCB and VFD L1,L2,L3 have two 75sqmm cable connected in each terminal.

 

QUERY -

1. if the Soft starter L1,L2,L3 got short circuit internally, will it affect the VFD's L1,L2,L3?

2. the rated tightening torque for VFD will differ if 2 cables are terminated in each terminals (L1,L2,L3)?


Pls suggest any problems in the present wiring and any good practice to be followed.

 

Rough sketch of wiring is attached.

Attachments
Labels
  • Labels:
  • Design & Build
  • Selection & sizing
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Werner_JUPPA
Crewman Werner_JUPPA Crewman
Crewman

Posted: ‎2022-06-02 10:20 PM

1 Like
1
2781
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
Posted: ‎2022-06-02 10:20 PM

 

Hello

 

These two devices probably never run at the same time, otherwise a common supply of 75mm² would be too small.

 

1. As soon as the Softstarter fails, the MCCB will trip and the VFD has no power supply anymore (and vice-versa).

2, Two wires of 75mm² each will probably fit in these terminals, but they are not designed for that. The terminals are designed for one wire with a maximum cross section of 120mm².

 

Basically, we would not recommend this wiring.

Either the two devices are powered individually by two MCCBs, or the two devices are protected locally with two circuit breakers (see attached drawing). These should be dimensioned in such a way that, in the event of a fault, the local CB switches off and not the MCCB. Both architectures are therefore redundant and the VFD remains in operation if the Softstarter should fail.

 

See Answer In Context

Attachments
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
Werner_JUPPA
Crewman Werner_JUPPA Crewman
Crewman

Posted: ‎2022-06-02 10:20 PM

1 Like
1
2782
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
Posted: ‎2022-06-02 10:20 PM

 

Hello

 

These two devices probably never run at the same time, otherwise a common supply of 75mm² would be too small.

 

1. As soon as the Softstarter fails, the MCCB will trip and the VFD has no power supply anymore (and vice-versa).

2, Two wires of 75mm² each will probably fit in these terminals, but they are not designed for that. The terminals are designed for one wire with a maximum cross section of 120mm².

 

Basically, we would not recommend this wiring.

Either the two devices are powered individually by two MCCBs, or the two devices are protected locally with two circuit breakers (see attached drawing). These should be dimensioned in such a way that, in the event of a fault, the local CB switches off and not the MCCB. Both architectures are therefore redundant and the VFD remains in operation if the Softstarter should fail.

 

Attachments
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

kishore1march
Lieutenant JG kishore1march
Lieutenant JG

Posted: ‎2022-06-06 09:24 PM

In response to Werner_JUPPA
0 Likes
0
2739
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
Posted: ‎2022-06-06 09:24 PM

Dear Werner,

 

This is a well guided answer. Thanks for your info and time. 

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

Preview Exit Preview

never-displayed

You must be signed in to add attachments

never-displayed
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.