Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum about SmartConnector applications for integration of other building management systems (BMS) into EcoStruxure Building Operation.
Search in
Link copied. Please paste this link to share this article on your social media post.
Hi all
Where is the documentation that explains how each swagger operation should be filled in? This is for SOAP REST API.
For example, what should it look like when I want to fill out the GET /Trends operation and try it out? What am I filling into these fields, using a real-life EBO example? The examples next to the field mean nothing to me.
I was able to GET and PUT values, so I got the basics. But the same input doesn't work for alarms or trends. In my basic EBO setup, I have 01%2FServer01%2FTest%2FStringValue. I also have an alarm in there too but I get a "doesn't exist" error when trying to get that alarms status.
Also, where do we have documentation for what you can and cannot do with SOAP REST API?
May anyone please advise on what this looks like in real life? The docs I've seen have no examples, just explanations of variables which, doesn't help. Thanks.
Link copied. Please paste this link to share this article on your social media post.
Hi Daniel,
If you are using the Get /Trends function, then you will most likely be getting the 'Bulk Retrieval not supported error'. That is because that feature is not supported and you can find plenty info about that message elsewhere on the forum
If you are after trend values, then use Get /Trend Samples and pass in the trend log path as the trendId parameter. See attached example.
If you actually want a list of trends objects in a folder, then use GET /Containers/{id}/Children where id is the folder path and is embedded into the URL as a double URL encoded query parameter.
Note, query parameters need to be double URL encoded and swagger interface only single encodes, so you need to single encode the path first before entering into the swagger interface. You can use an online converter to do this. e.g. https://www.urlencoder.io/
Hope this helps!
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.