2022-12-09
07:57 AM
Swagger Curl issue
Hi,
With the SmartConnector, when we use swagger, we can have a curl syntax.
We would like to use that curl syntax to test it.
It seems that for a PUT operation the given syntax is not good.
Here are our tests:
It woks with swagger.
Now with the Curl command, the Get works, but the PUT fails (reset value to 0):
Do you have an idea what is the correct curl syntax for that case ?
We already tried (without success):
Thanks,
Bertrand
Replies 0