Smart Connector - Server Connections

SmartConnector Forum

Schneider Electric support forum about SmartConnector applications for integration of other building management systems (BMS) into EcoStruxure Building Operation.
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
  • EcoStruxure Building
  • SmartConnector
  • SmartConnector Forum
  • Smart Connector - Server Connections
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
JeffBowman
Sisko JeffBowman Sisko
164
sesa180908_brid
Commander sesa180908_brid Commander
34
ardak
ardak Schneider Alumni (Retired)
34
View All

Recommended Forums

  • Intelligent Devices Forum

  • Metering & Power Quality

  • EcoStruxure IT Forum

Related Products
product field
Schneider Electric
Smart Connector
product field
Comfort Laboratory
SmartConnector SNMP Extension
product field
Comfort Laboratory
SmartConnector OPC Classical Extension

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to SmartConnector Forum
Start a Topic
Solved
Alvaro_Olarte
Crewman Alvaro_Olarte Crewman
Crewman

Posted: ‎2020-10-13 10:26 PM

0 Likes
3
2299
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
‎2020-10-13 10:26 PM

Smart Connector - Server Connections

Hello,

 

I have the following questions about Smart Connectors:

 

1. Can a smart connectors be added to an Enterprise Central? I have review the EC specification sheet and there is no option for smart connectors as add-ons. It only seams to be available for ES and AS.

 

2. If we need to communicate a ES or EC using two smart connectors, one smart connector to read data from an SNMP network and another smart connector to connect to an OPC server, besides of the individual licenses for each smart connector, How many framework licenses (SXWSWSCDL100001) do we need? just one or two.

 

3. Is it possible to install the smart connector service on a different server of the ES?

  • Thumbnail of Smart Connector
    Schneider Electric
    Smart Connector
  • Thumbnail of SmartConnector OPC Classical Extension
    Comfort Laboratory
    SmartConnector OPC Classical Extension
  • Thumbnail of SmartConnector SNMP Extension
    Comfort Laboratory
    SmartConnector SNMP Extension
View products (3)
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
JeffBowman
Sisko JeffBowman Sisko
Sisko

Posted: ‎2020-10-14 07:25 AM

1 Like
2
2286
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
‎2020-10-14 07:25 AM

Hi @Alvaro_Olarte,

 

To answer your questions:

 

1. Yes, Smart Connector works with the EC.

2. If you need to work with multiple different Smart Connector extensions, you should be able to install both on the same Smart Connector instance. So you will only need 1 framework license. However, if you want to install them on two different PC's, you will need 2. You will also need to get the licenses for the extensions themselves.

3. Yes, it is possible to install Smart Connector on a different computer. We generally recommend installing Smart Connector on the same machine as EBO, as the PC already exists, so in most cases it makes sense to use it, but it can in theory be installed anywhere that has network access to EBO.

 

Best Regards,

 

-Jeff

See Answer In Context

Tags (1)
  • Tags:
  • english
Reply
Replies 3
JeffBowman
Sisko JeffBowman Sisko
Sisko

Posted: ‎2020-10-14 07:25 AM

1 Like
2
2287
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
‎2020-10-14 07:25 AM

Hi @Alvaro_Olarte,

 

To answer your questions:

 

1. Yes, Smart Connector works with the EC.

2. If you need to work with multiple different Smart Connector extensions, you should be able to install both on the same Smart Connector instance. So you will only need 1 framework license. However, if you want to install them on two different PC's, you will need 2. You will also need to get the licenses for the extensions themselves.

3. Yes, it is possible to install Smart Connector on a different computer. We generally recommend installing Smart Connector on the same machine as EBO, as the PC already exists, so in most cases it makes sense to use it, but it can in theory be installed anywhere that has network access to EBO.

 

Best Regards,

 

-Jeff

Tags (1)
  • Tags:
  • english
Reply
Erwin-vd-Zwart
Janeway Erwin-vd-Zwart Janeway
Janeway

Posted: ‎2020-10-14 07:29 AM

0 Likes
1
2284
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
‎2020-10-14 07:29 AM

@JeffBowman I can recall the DB needs to be on the same machine as the SC correct?

Tags (1)
  • Tags:
  • english
Reply
JeffBowman
Sisko JeffBowman Sisko
Sisko

Posted: ‎2020-10-14 07:44 AM

0 Likes
0
2281
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
‎2020-10-14 07:44 AM

Hi @Erwin-vd-Zwart,

 

Kind of true.


This is only true if you are using SQLEXPRESS for the database. In that case the Database needs to be on the same machine as Smart Connector.


If you use a full SQL server install, then the database does not need to be on the same machine.

 

Best Regards,

 

-Jeff

Tags (1)
  • Tags:
  • english
Reply
Preview Exit Preview

never-displayed

You must be signed in to add attachments

never-displayed
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.