Ask our Experts
Didn't find what you are looking for? Ask our experts!
Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Schneider Electric support forum about SmartConnector applications for integration of other building management systems (BMS) into EcoStruxure Building Operation.
Search in
Link copied. Please paste this link to share this article on your social media post.
I just installed SQL2012 Express and SmartConnector. SmartConnector service is not starting, and provides the following error:

I found the following post, and checked the logs:
SmartConnectorService can not start
The .log file attached contains the info. It appears there was some user/password snafu, and I am unsure how that gets established.
For some background, I have attempted this several times, working on this for the past 8 hours. I have Installed and uninstalled this 4 times, using SQL2017 (which I then realized was not supported), SQL2016 (which had this same problem of not starting the service), and now SQL2012. I just clicked through the basic, default SQL installation (including adding a check to 'LocalDB'), then followed the 'Installation and Configuration Guide'. I did the 'Complete Install', and set this exactly as seen, making the password 'admin':

I am ridiculously unsure how the DB should be configured, and the install guide is unclear. Would it be possible to get a set of queries to configure SQL as it should be? Is there some better guide for the SQL part of this?
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
EDIT:
~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
I got this working. I did a few things; I am not sure which one actually worked.
First off, I used the SqlExpress Server Type in the SmartConnector install, instead of LocalDB. (I had both installed, but I guess LocalDB wasnt wanting to work...) I used 'Windows Implicit' Authentication (just trying to develop things ATM), and it started throwing a new error in the logs, and actually installed the DB, but it still seemed to be a permissions problem.
I found this post - iis - SQL Server Login error: Login failed for user 'NT AUTHORITY\SYSTEM' - Stack Overflow - (ALL HAIL StackOverflow!!), and made the 'NT AUTHORITY\SYSTEM' user the sysadmin of the DB. This FINALLY got the service running when I then reinstalled SmartConnector. However, when I browsed to 'localhost:8082', it was no dice.
So, I thne remembered seeing this post at some point during the day - Enable remote connections for SQL Server Express 2012 - Stack Overflow - (Seriously. HAIL. THEM.) I started the SQL browser service, and I am now about to attempt a login.
Now that step 1 is done, maybe I will not have to come back. Maybe. Only 60 pages of install and config to go. (One can hope...)
Link copied. Please paste this link to share this article on your social media post.
Hi Lucas,
I am glad you were able to work through your install issues on your own!
Let me see if I can shed some light onto what you were experiencing.
The next part of it, where after using 'Windows implicit' credentials and then receiving the permissions error for NT AUTHORITY\SYSTEM, after looking into it, I actually think that this part of it is a bug in the installer. When using the Windows implicit login types, the installer should be setting up the System user permissions in the database, and making sure the SYSTEM user doesn't need elevated SQL permissions besides 'db_owner' on the SmartConnector database. In inspecting the installer code, although the code that does this exists, it is not being executed when the installer runs.
Overall though! I think you may have gotten over the hardest part
(harder than it should have been for sure, the installer will be fixed going forward.) Once the service is installed, running, and licensed, I hope understanding the configuration will be more straight forward for you!
Thank you for reaching out!
Regards,
-Jeff
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.