Hi Steve,
There have been some reports (about 3, including yours) lately of the machine thumbprint changing on a PC reboot... I have no idea what could be causing this! All these reports have come in the past few weeks, so I am wondering if there was some windows update that is causing this issue.. The machine thumbprint is a hash of the MAC Address(s) on the machine, as well as the serial number of the motherboard.
I don't believe the MAC addresses are the issue here as when we check the thumbprint we are actually generating every possible thumbprint with each MAC address to make sure we are valid if the active MAC address changes. So I am thinking there is something weird going on with the serial number of the Motherboard on reboot..
I checked the source code, and we don't add anything to the log when we create the thumbprint (probably for security purposes.. so it would be difficult to debug this in the field, to see if there is something wrong with the Serial number/ MAC address that could be causing the thumbprint to change.
That said, I would be happy to create a incremental build with some logging added, if you would be willing to install it and help me run some tests (I haven't been able to reproduce this defect locally on any of my machines).
Best Regards,
-Jeff