Ask Me About Webinar: Data Center Assets - Modeling, Cooling, and CFD Simulation
Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!
SmartConnector Forum
Schneider Electric support forum about SmartConnector applications for integration of other building management systems (BMS) into EcoStruxure Building Operation.
Link copied. Please paste this link to share this article on your social media post.
I am using EWSClient to read all the SBO alarm Objects from
the SBO System tree. I need to find out the Category for the Alarm for my
configuration processor. The AlarmItemType object doesn’t have category
information and I did not found any API in EWSClient to get category
information for an alarm Item.
I wonder if there is any API in EWS Client to get the
category for an alarm item? Or smartconnector methods to retrieve complete
alarm item information or AlarmEventsType object using AlarmItem Id.
I did try ewsClient.getItems(alarmId), however that returns same
AlarmItemType object.
Any thoughts?
Thanks!
Neeraj Tomar
Link copied. Please paste this link to share this article on your social media post.
Hi Neeraj,
I don't believe what you are trying to do is possible via EWS. While it's possible to get the list of AlarmEventTypes that are currently in the server, there is no way to get the AlarmEventType per AlarmItem, this is because in EWS an AlarmItem is not confined to a single AlarmEventType (although this is how SBO implements it Internally.)
To go further on the above, the EWS AlarmItem does not contain a property for the AlarmEventType as this is specific to the AlarmEvent itself. In fact, in the EWS world, multiple AlarmEventTypes could in theory be used from an AlarmItem is triggered into alarm to when it is finally returned back to normal, and there would be nothing wrong in doing it this way. However, the way SBO implements AlarmEventType (Category) is to have it a single category bound to the Alarm Object. So even though you know this value is static through the AlarmEvent cycle, there is no way to get this from the AlarmItem itself via EWS.
Regards,
-Jeff
Link copied. Please paste this link to share this article on your social media post.
Neeraj,
What SBO shows as "Category" in the Alarm Viewer window, is the AlarmEventType in EWS parlance.
If you review section 4.6.2 (specifically table 14) from the EWS Specification (https://www.smartconnectorserver.com/DownloadCenter/Contents/ews) you will see that an AlarmEvent has a "Type" property (aka an SBO category).
The EwsClient supports retrieval of all AlarmEventType defined by a server by using the "GetAlarmEventTypes" method (see section 5.6.4).
M
Link copied. Please paste this link to share this article on your social media post.
That I know. I am actually talking about reading alarm definition from the SBo tree and not the triggered alarm in Alarm viewer. I need to know alarm item category or type even before alarm is triggered for my project.
For Example – If an Alarm is defined in SBo as ‘matching text
string alarm’:
Name – ‘ChillerFlowRateAlarm’,
Description - High Temperature Failure for Chillar Plant #1
Category - ~/System/Alarm Control Panel/AlarmHandling/Categories/Chiller Plant #1
Alarm Message - Chiller Flow Rate Failure for Chillar Plant#1
Monitored Variable - ../../CMMSPoints/ChillerFlowRate/Value
This alarm has never been triggered. No Alarm history or instance in alarm viewer. So, When I read this item, I get AlarmItemType object that doesn’t have category information. I know that if there is alarm history I can get type from there. However, there is no history or actual alarm happened yet. It's at the configuration part of the project.
Do you know about how to retrieve category at this point?
Link copied. Please paste this link to share this article on your social media post.
Hi Neeraj,
I don't believe what you are trying to do is possible via EWS. While it's possible to get the list of AlarmEventTypes that are currently in the server, there is no way to get the AlarmEventType per AlarmItem, this is because in EWS an AlarmItem is not confined to a single AlarmEventType (although this is how SBO implements it Internally.)
To go further on the above, the EWS AlarmItem does not contain a property for the AlarmEventType as this is specific to the AlarmEvent itself. In fact, in the EWS world, multiple AlarmEventTypes could in theory be used from an AlarmItem is triggered into alarm to when it is finally returned back to normal, and there would be nothing wrong in doing it this way. However, the way SBO implements AlarmEventType (Category) is to have it a single category bound to the Alarm Object. So even though you know this value is static through the AlarmEvent cycle, there is no way to get this from the AlarmItem itself via EWS.
Regards,
-Jeff
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.
With achievable small steps, users progress and continually feel satisfaction in task accomplishment.
Usetiful Onboarding Checklist remembers the progress of every user, allowing them to take bite-sized journeys and continue where they left.
of