Alarm transfer to EBO from SmartConnector DB using the EWS Server

SmartConnector Forum

Schneider Electric support forum about SmartConnector applications for integration of other building management systems (BMS) into EcoStruxure Building Operation.
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
  • EcoStruxure Building
  • SmartConnector
  • SmartConnector Forum
  • Alarm transfer to EBO from SmartConnector DB using the EWS Server
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
JeffBowman
Sisko JeffBowman Sisko
164
ardak
ardak Schneider Alumni (Retired)
34
sesa180908_brid
Commander sesa180908_brid Commander
34
mike_meirovitz
Commander mike_meirovitz
21
View All

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to SmartConnector Forum
Start a Topic
Solved
sesa379286_brid
Ensign sesa379286_brid Ensign
Ensign

Posted: ‎2018-04-06 12:48 AM

0 Likes
1
1372
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
‎2018-04-06 12:48 AM

Alarm transfer to EBO from SmartConnector DB using the EWS Server

Hello to all,

I am trying to understand the structure an alarm should have in the SmartConnector Db (I have already done it with success for EWSValueItems and HistoryItems). When I create an EWSAlarmItems i see in SBO the message attached.

I believe that this has to do with the transition model or another parameter in the system.

Can you provide me with an example to test before moving to the worker development?

Thank you

Attachments
Tags (3)
  • Tags:
  • database
  • ebo alarms
  • ewsalarms
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
JeffBowman
Sisko JeffBowman Sisko
Sisko

Posted: ‎2018-04-17 01:00 PM

0 Likes
0
1323
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
‎2018-04-17 01:00 PM

Hi Sotiris,

Sorry for the delayed response, I actually didn't even see this post until now.

It is hard for me to understand what is occurring here, how are you going about creating these in the database? Are you simply adding them via the Smart Connector portal? Or are you doing it via code?

If you are doing it via code, there are already functions you can use to add them to the database for you, so in theory you don't need to worry about how it looks in the database.

From the error in SBO it looks as though your Smart Connector EWS Server is responding with an internal server error. Are you able to turn on EwsServe logging, and see if you can see what this error is?


Regards,

-Jeff

See Answer In Context

Reply
Reply 1
JeffBowman
Sisko JeffBowman Sisko
Sisko

Posted: ‎2018-04-17 01:00 PM

0 Likes
0
1324
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
‎2018-04-17 01:00 PM

Hi Sotiris,

Sorry for the delayed response, I actually didn't even see this post until now.

It is hard for me to understand what is occurring here, how are you going about creating these in the database? Are you simply adding them via the Smart Connector portal? Or are you doing it via code?

If you are doing it via code, there are already functions you can use to add them to the database for you, so in theory you don't need to worry about how it looks in the database.

From the error in SBO it looks as though your Smart Connector EWS Server is responding with an internal server error. Are you able to turn on EwsServe logging, and see if you can see what this error is?


Regards,

-Jeff
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.