Wiser 3 phase Power tag measuring half of the actual load
Schneider Electric Wiser Forum
Connect with Wiser Smart Home solution experts in the Schneider Electric Wiser forum. Discuss tips on features, updates, installation, and how to get the most out of your Wiser products.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2023-10-1611:08 PM
Wiser 3 phase Power tag measuring half of the actual load
Hello!
I have a couple of Wiser power tags, 3 phase A9F63 flex 3 phase, connected to a Gateway.
The power tags are measuring exactly half of what I expect. For example if I, for the sake of testing, just plug in a 800W radiator over night and nothing else, I get readings of 400W instant power and 0.4kWh every hour. The same regardless if I configure the power tag as grid or something else.
One thing I have noticed, is that the power tag cables (which is powering the tag itself I assume) are not connected directly on the same cables that run through the tag, but on a separate power group. Not sure if that could have an impact?
I reside in Sweden, with a 230V grid.
Does anybody know what could be the cause of this issue?