Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84865members
354354posts

Square D X series outlet Monitoring solution

Schneider Electric Wiser Forum

Connect with Wiser Smart Home solution experts in the Schneider Electric Wiser forum. Discuss tips on features, updates, installation, and how to get the most out of your Wiser products.

BigBillSD
Ensign
Ensign
0 Likes
5
399

Square D X series outlet Monitoring solution

I have looked all over the se.com website and still cannot figure out what software/hardware is needed to monitor the power of the X series outlets and switches.   I have asked on reddit and other similar forums.  One person thinks it the Wiser app so I am here.  Is there any documentation on what works with those outlets and switches?   I have finding it hard to believe I haven't been able to find anything after 4 hours of searching.  I did finally find a techhive article, but there was barely any info in that. 

 

I have seen a lot of reviews of the Sense app and even after 5 months of use on the last video 76% of the power being used still showed it as being "Other" which was pretty incredible as they guy never mentioned the elephant in the room..

 

Please point me to some documentation with respect to how to monitor the X series plug and switches. 

 

-Bill

Tags (2)
5 Replies 5
sesa505826_brid
Cadet
Cadet
0 Likes
1
373

Re: Square D X series outlet Monitoring solution

You can find more details about our connected offers at this page, https://shop.se.com/us/en/. We need the Wiser Home app from SE to commission and manage the Sqaure D connected Wiring devices, https://shop.se.com/us/en/connected-home/switches-sensors-outlets

 

The Wiser Energy (Sense) monitor is integrated to the Sqaure D connected Wiring devices, If you have the Wiser Energy Monitor installed, you can use the Sense app to control these devices once you enable the integration. 

Tags (1)
BigBillSD
Ensign
Ensign
0 Likes
0
367

Re: Square D X series outlet Monitoring solution

I followed the two links, but that is what I already found, extremely high level marketing stuff.  Nothing that explains what is possible and what is needed to make it all work.  Nothing about how many outlets or switches there can be.  Nothing about whether they connect to WiFi via WPA3 or god forbid WEP.  No capabilities etc.  All just marketing fluff.  Did I miss the link with real information?  Its not like we can call an electrician and expect them to have a clue about the monitoring piece of the puzzle.  Calling a plumber would be just as helpful.  -Bill

Tags (1)
kkranen
Crewman
Crewman

Re: Square D X series outlet Monitoring solution

Hi @BigBillSD 

 

I'm a Sense (Wiser Energy is rebranded version of Sense) and use both TP-Link/Kasa and Wiser smartplugs with Sense.  A few answers to your questions.

  • For me, the Sense (Wiser Energy) has been a great energy saver and I'm only seeing about 20% in Other.  Sometimes more and sometimes less.  I do use quite a few smartplugs (10 or so) to reduce Other.

    IMG_E9246EE1A36E-1.png
  • I current prefer the TP-Link/Kasa smartplugs to the Wiser X-Series smartplugs, because the Wiser X-Series have a known issue when providing realtime data - they occasionally transmit spurious ridiculously high measurements to the Sense / Wiser Energy measurments.  Here's an example - 16kW spikes from a 4W electronic device.

    Wiser EnergyWiser Energy

  • I do like the Wiser X-Series switches because they allow me to add measurement to devices (ceiling lighting, etc.) I can't put on smart pugs.  Double good because the Wiser integration with Sense/Wiser Energy doesn't put an additional local load on the Sense monitor - it's all cloud to cloud. 
  • I'm using the X-Series with WPA2.  All the devices are 2.4GHz so they live on my IoT network and SSID. 

 

Let me know if you have more questions.

Tags (1)
BigBillSD
Ensign
Ensign
0 Likes
1
206

Re: Square D X series outlet Monitoring solution

Thanks for your reply.  I will have to figure out how to get those charts you put in the post.     I started working with the Emporia Energy dev team on getting their smart-plugs to connect via WPA3, they were successful a couple months back and have now standardized on their smart plugs.  Their mobile interface is currently a lot better than the Wiser one, but hopefully they will continue to work on that  I was happy when they added relative time scheduling a few months back to the app.   There is still a long way to go.  The SquareD switches and outlets work flawlessly on WPA3 so that is a good thing.  The sense app is painfully slow at adding devices.  To actually make it useful it needs a way for advanced users to be able to train it.  That seems like a glaring hole in the product.  Its been many months now, and has hardly found but a few lights and a fridge.  And that is plugged into one of the SqD outlets and a bug makes it think its out there twice.  I logged a ticket a few months ago, no response since. 

 

My wiser circuit breaker device is still fairly useless for me as it cannot deal with they type I have.  There is no way to put clamps around the mains.  They are buss bars and very little space around them.   I was able to use the Emporia Energy panel device as they have multiple ways to get the mains data.  I chose to use their Smart-meter Zigbee connection as the incoming power meter instead of the hardwired CT's.   Even EE's optional flexible CT loops couldn't fit behind the buss bars of my main circuit panel.  

So my Wiser (sense) box is relegated to see one sub panels 100 amp input  Less than 60% of the home circuits are on that sub-panel.    The other issue with the current W/S box is it cannot do WPA3, so putting it out near the street is problematic due to constant war driving in big cities. 

Tags (1)
kkranen
Crewman
Crewman
0 Likes
0
204

Re: Square D X series outlet Monitoring solution

Interesting. I investigated Emporia a year or so ago, but I have way too many individual circuits in my house and the packing is way too tight to get the coverage I get out of Sense / Wiser Energy.  If I want to do the whole CT per circuit thing, I'll move to a SPAN. I don't really care WPA2 or WPA3 today. 

I think the big challenge with Sense is that the users "mileage" varies by household. As I said, I'm seeing only about 20% Other, but others see 50%. Sense sees my EV charging and AC usage, but other EV models can be more problematic.  My system performs well and I'm quite happy. My only beef is that the Wiser X Series is prone to throwing off huge, obviously wrong, energy spikes that aren't visible in the Wiser App, but do show up in the associated Power Meter for that device in the Wiser Energy / Sense app. 

Two other things I like about the Sense world.  Sense has a built-in integration with Home Assistant so I can pull together data from all my IoT devices to monitor home efficiency - Here's Sense power data on top and Ecobee thermostat setting, temperature and run command data on the bottom. 

Screen Shot 2022-08-09 at 3.19.58 PM.png

 

Second, Sense has branched out in smart panels (through Square D) and into meters (through Landis & Gyr).  That means they will have hundreds of thousands of installs within a few years.

Glad your environment is working well you. 

Tags (1)