Missing an important Push Button Dimmer Toggle Mode feature
Schneider Electric Wiser Forum
Connect with Wiser Smart Home solution experts in the Schneider Electric Wiser forum. Discuss tips on features, updates, installation, and how to get the most out of your Wiser products.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-11-2307:50 AM
Missing an important Push Button Dimmer Toggle Mode feature
I have a Push Button Dimmer with the On & Off buttons with dimmer side by side and two additional Moment buttons underneath.
I would like to I would like to set the default dimmer value to a fixed value less than 100%, so that every time I press the On button it will light with this pre-set dimming percentage. Today this is not possible.
The Toggle Mode setting options I have are:
100% or
Last Level
A third option should be added to set default dimmer level to a value less than 100% !!
Here is the issue:
I find the 100% level too bright for the Lamp used where it is placed + plus I like to be eco friendly and save some power. I can of course set the Toggle Mode to Last level and set the Dimmer % to my preferred value (e.g. 50%). However if I use on of the Moments Buttons to control the same Lamp and use a different Dimmer % (e.g. 25%) for this Button, then when the Lamp is turned off, it will become the 25% Dimmer value that becomes the Last Level, and next time I turn on the Lamp it will turn on at 25%.
I have tried to set the Dimmer range to max at my 50% Level, but if Toggle Mode is set to 100%, it will overrule the Dimmer range setting.
Can we please get this feature added to Toggle Mode or have anyone figured out a good way of overcoming this issue? Help me please 🙂