Ask our Experts
Didn't find what you are looking for? Ask our experts!
Connect with Wiser Smart Home solution experts in the Schneider Electric Wiser forum. Discuss tips on features, updates, installation, and how to get the most out of your Wiser products.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-11-24 04:46 AM
I've recently picked up a Gen1 HubR, a room thermostat and several radiator thermostats. The control of the room with the room thermostat has been stellar; however, the rooms with only radiator thermostats are struggling to get accurate/sensible readings. I have the Wiser system paired with my Home Assistant instance, so I've been able gather quite a bit of data. Each room also has a Zigbee temp sensor paired with home assistant that I've calibrated with a traceable thermometer, so I'm pretty happy with the readings they give me. When the radiator valves are open, the temp reported by the iTRV is usually 2 to 2.5 degrees above the actual room temp. I've seen lots saying just make the set point 2 degrees higher, which is ok when valve is frequently opened, but doesn't work when I lower the temp by a few degrees over night. In that case, the iTRV and actual room temperatures eventually converge, and the artificially boosted set points means the the thermostat will begin heating 2 degrees higher than it needs to. I suppose the overnight set point could be at the actual desired temp while the daytime setting would be elevated by 2 degrees, but this again falls apart e.g. on an exceptionally cold night (where the radiator is warm most of the time, so the readings will be high) or on warmer days (where there isn't much demand for heat, so the reading is actually close to the actual temp). I've also noticed some odd behavior in the temp readings. Sometimes, there will be a prolonged period of steady demand and the iTRV's reading steadily increases. Other times, the valve will open for 2 minutes, and the reading will spike by a degree and stay there for almost an hour, keeping valve from demanding heat again for quite a while. Meanwhile, the actual room temperature continues to fall because of it. The attached plots demonstrate all of these behaviors. During this time period, the boiler is being controlled in relay mode (as a gas boiler) with a 60 degree flow temp. I'm seeing the same behavior with Opentherm, but I wanted to eliminate some of that complexity while debugging.
Has anyone found a solution for this save needing to spend a considerable amount on a room thermostat for every room?
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-11-27 03:40 AM
Hi @astephon88 ,
Thanks for your post. As the iTRV is mounted on the radiator, it is normal that we report some temperature readings gaps with other sensors. We recommend to install in addition, a Room Thermostat in the roon to obtain a more accurate temperature.
BR
David
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-11-28 12:06 AM
@David_SE thanks, but as I mentioned, I was hoping for a solution that doesn't involve spending another £400 on room thermostats.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2025-12-03 01:51 AM
Hi, Do you have open window detection turned on? That sometimes (not exactly meets the description you give) does affect the setpoints.
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.