Ask Me About Webinar: Data Center Assets - Modeling, Cooling, and CFD Simulation
Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!
Protection & Control
Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
Link copied. Please paste this link to share this article on your social media post.
Hi everyone,
As one of the solutions, we use Saitel DP as an RTU for MV SS.
Ad its normal features:
* getting information from relays over communication (IEC61850 most common);
* information by DI/DO/AI ;
* sending these information to the upper level SCADA system by protocol ;
* receiving commands from upper level SCADA. (IEC101, IEC104...) ;
And now we get to the main point. There is need that in some conditions like when main local/remote switch in SS is in LOCAL state, all the commands from upper level SCADA that comes to Saitel should be blocked and/or not executed. Example: SCADA sends over IEC104 command to Saitel, and Saitel sends over IEC61850 open/close command to IED
So we have lets say digital input wired on Saitel that signals that main local/remote switch is in LOCAL, and we need to block remote commands that comes to the Saitel and/or to be executed to the IED.
Anyone done similar thing or any idea witch signal in Saitel can be used for this?
Similar thing can be for Saitel DR, or even maybe T300, as they are on same platform/software,
Best regards,
Link copied. Please paste this link to share this article on your social media post.
In status table:
GECC02_GATE_SUBST_MODE | SUBSTATION MODE | Formula | GECC02_GATE_SUBST_CMD | TSGTW01 | [TSGTW01SYSTEM/LLN0$ST$RemLoc$]stVal:q:t | 1 | False | False | False | False |
in cmd table:
GECC02_GATE_SUBST_CMD | SUBSTATION MODE COMMAND | TSGTW01 | [TSGTW01SYSTEM/LLN0$CO$RemLoc$] | SCADA | 200296:CSC | Formula | GECC02_GATE_SUBST_MODE:EVENT | SOE | GECC02_GATE_SUBST_CMD:YES | False |
Where:
SCADA is the 104 channel
TSGTW01 is the saitel it-self.
Best Regards
Link copied. Please paste this link to share this article on your social media post.
In status table:
GECC02_GATE_SUBST_MODE | SUBSTATION MODE | Formula | GECC02_GATE_SUBST_CMD | TSGTW01 | [TSGTW01SYSTEM/LLN0$ST$RemLoc$]stVal:q:t | 1 | False | False | False | False |
in cmd table:
GECC02_GATE_SUBST_CMD | SUBSTATION MODE COMMAND | TSGTW01 | [TSGTW01SYSTEM/LLN0$CO$RemLoc$] | SCADA | 200296:CSC | Formula | GECC02_GATE_SUBST_MODE:EVENT | SOE | GECC02_GATE_SUBST_CMD:YES | False |
Where:
SCADA is the 104 channel
TSGTW01 is the saitel it-self.
Best Regards
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.
With achievable small steps, users progress and continually feel satisfaction in task accomplishment.
Usetiful Onboarding Checklist remembers the progress of every user, allowing them to take bite-sized journeys and continue where they left.
of