Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Saitel RTUs - Hot-standby using WiFi communication between two Saitel CPUs?

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • Saitel RTUs - Hot-standby using WiFi communication between two Saitel CPUs?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Araceli_Monje Mentor
74
JuanRayo
JuanRayo Mentor
38
Arun-kumar_PS
Arun-kumar_PS Mentor
33
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
sesa426102_brid
sesa426102_brid Leader
Leader

Posted: ‎2020-04-05 10:47 PM . Last Modified: ‎2024-07-05 01:14 AM

0 Likes
4
1993
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
‎2020-04-05 10:47 PM

Saitel RTUs - Hot-standby using WiFi communication between two Saitel CPUs?

Is it possible to have 2 Saitel RTUs as a Hot standby arrangement connected on a wireless network? If Yes, what part number should we refer to?

Labels
  • Labels:
  • Saitel range
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Iván_González
Iván_González Mentor
Mentor

Posted: ‎2020-04-06 11:27 PM

1 Like
0
1972
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
‎2020-04-06 11:27 PM

Morning Michael,

 

Redundant Saitel DP CPUs can be installed in the same rack or different racks. When installed in the same rack, they can share serial expansion modules and manage redundancy data using dedicated backplane lines.

 

Regarding the redundancy mechanism there are two different aspects:

  • CPU coordination makes us of two physical channels. These can be backplane lines, serial or ethernet ports.
  • CPU data synchronization can make use of dedicated backplane or an ethernet port. WiFi links should be alright for this.

See Answer In Context

Tags (1)
  • Tags:
  • Saitel Ethernet Redundancy
Reply
Replies 4
sesa426102_brid
sesa426102_brid Leader
Leader

Posted: ‎2020-04-05 11:03 PM

0 Likes
0
1990
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
‎2020-04-05 11:03 PM

And, because wifi has bandwidth issue or latency issue, is it still possible to use 2 Saitel RTUs on a Hot standby arrangement. This is for a project specifying the hot standby arrangement as a mandatory requirement.

Reply
Iván_González
Iván_González Mentor
Mentor

Posted: ‎2020-04-05 11:31 PM

2 Likes
2
1988
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
‎2020-04-05 11:31 PM

Hello there. Saitel CPUs do not have embedded wifi ports - only copper or fiber ehternet links are supported.

 

In any case, the HOT-STANDBY functionality of Saitel CPUs is designeed to maximise uptime of the redundant system by having the 2 CPUs share the same databse and configuration. Only the  HOT CPU will be actively communicating and acquiring data, with the STANDBY one receiving updated information from the HOT one.

 

In that type of setup, each port (serial or ethernet) can be connected to wireless modems and redundant communication links configured to make use of these.

Tags (1)
  • Tags:
  • Saitel
Reply
michael_mckay_p
michael_mckay_p
Explorer

Posted: ‎2020-04-06 08:43 PM

1 Like
1
1976
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
‎2020-04-06 08:43 PM

Thanks Ivan,

 

Do the 2 CPUs have to be in the same rack? Is that correct? If so, can the CPU synchronization happen effectively over an Ethernet network with a wifi segment?

Reply
Iván_González
Iván_González Mentor
Mentor

Posted: ‎2020-04-06 11:27 PM

1 Like
0
1973
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
‎2020-04-06 11:27 PM

Morning Michael,

 

Redundant Saitel DP CPUs can be installed in the same rack or different racks. When installed in the same rack, they can share serial expansion modules and manage redundancy data using dedicated backplane lines.

 

Regarding the redundancy mechanism there are two different aspects:

  • CPU coordination makes us of two physical channels. These can be backplane lines, serial or ethernet ports.
  • CPU data synchronization can make use of dedicated backplane or an ethernet port. WiFi links should be alright for this.
Tags (1)
  • Tags:
  • Saitel Ethernet Redundancy
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.