Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

SEPAM B83 replacement Powerlogic P5 / P7

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • SEPAM B83 replacement Powerlogic P5 / P7
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Commander Araceli_Monje Commander
43
Arun-kumar_PS
Commander Arun-kumar_PS Commander
21
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
sesa211247_brid
Lieutenant sesa211247_brid Lieutenant
Lieutenant

Posted: ‎2024-05-03 12:56 PM

0 Likes
4
1227
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
‎2024-05-03 12:56 PM

SEPAM B83 replacement Powerlogic P5 / P7

Dear Community, 

 

Is there any plan to replace the SEPAM B83 IED within the Powerlogic P5 / P7 range

 

until now there is no IED that replace the SEPAM B83 ! 

SEPAM B83 is very helpful when syncing 2 busbar using the ANSI27 protection on each parts of the busbar 

Labels
  • Labels:
  • Application cases
  • IEC61850
  • PowerLogic P5
  • PowerLogic P7
  • Sepam range
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Stefan_Scharf
Ensign Stefan_Scharf Ensign
Ensign

Posted: ‎2024-08-16 12:30 AM

0 Likes
2
1062
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
‎2024-08-16 12:30 AM

There is no 1:1 replacement for SEPAM B83. You can use PowerLogic P7 for this application e.g. Feeder application level 1 supporting 2x 3phase VT proxies or 2x 1ph VT proxies. Sync-check ANSI 25 is also available. However, sufficient number of VT inputs are needed, you can choose between two CT/VT module variants 5CT/4VT or 6CT/3VT - max two modules are possible.

See Answer In Context

Reply
Stefan_Scharf
Ensign Stefan_Scharf Ensign
Ensign

Posted: ‎2024-08-19 01:09 AM

1 Like
0
1014
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
‎2024-08-19 01:09 AM

It is available. When using e.g. P7 Feeder 2x 3ph VT  and 2x 1ph VT proxies are supported which is meeting B83 requirement which is 2x 3V + 2x V0 acc to SEPAM catalog. You have to make sure that the needed CT/VTs are equipped. Up to two CT/VT moudles can be equipped.

See Answer In Context

Reply
Replies 4
Stefan_Scharf
Ensign Stefan_Scharf Ensign
Ensign

Posted: ‎2024-08-16 12:30 AM

0 Likes
2
1063
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
‎2024-08-16 12:30 AM

There is no 1:1 replacement for SEPAM B83. You can use PowerLogic P7 for this application e.g. Feeder application level 1 supporting 2x 3phase VT proxies or 2x 1ph VT proxies. Sync-check ANSI 25 is also available. However, sufficient number of VT inputs are needed, you can choose between two CT/VT module variants 5CT/4VT or 6CT/3VT - max two modules are possible.

Reply
sesa211247_brid
Lieutenant sesa211247_brid Lieutenant
Lieutenant

Posted: ‎2024-08-17 03:25 PM

0 Likes
1
1041
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
‎2024-08-17 03:25 PM

Thank you for your response,

but without 2 voltages inputs on the P7 we can not achieve the 27R function on each busbar.

as you know this function is mandatory to make sure that there in no remanent energy (voltage) coming from motors during the CB's switching.

this could be solved if the P7 can handle 6 VT inputs (3 on each busbar).

 

Hope our colleague from R&D will manage this in the near future. 

Reply
Stefan_Scharf
Ensign Stefan_Scharf Ensign
Ensign

Posted: ‎2024-08-19 01:09 AM

1 Like
0
1015
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
‎2024-08-19 01:09 AM

It is available. When using e.g. P7 Feeder 2x 3ph VT  and 2x 1ph VT proxies are supported which is meeting B83 requirement which is 2x 3V + 2x V0 acc to SEPAM catalog. You have to make sure that the needed CT/VTs are equipped. Up to two CT/VT moudles can be equipped.

Reply
sesa211247_brid
Lieutenant sesa211247_brid Lieutenant
Lieutenant

Posted: ‎2024-08-19 01:34 AM

0 Likes
0
1005
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
‎2024-08-19 01:34 AM

Thank You 

I'll check-it
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.