Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hello everyone,
In my current T300 project, if the IEC 104 channel is broken then the IEC 101 one should start running.
Link copied. Please paste this link to share this article on your social media post.
Hi Milica
Would be very useful to know your real application case as requested by Jean-Yves
Is there any legacy habit there?
Generally speaking, it is SCADA/Client responsibility to switch from one channel to another: therefore there is no automatic switching for IEC104/ 101 at T300 level.
The link notion referred by Manuel is applicable to DNP3 protocol
Best Regards
Link copied. Please paste this link to share this article on your social media post.
Hi Milica,
In T300 catalogue, page 29 you can find:
Channel association - Links
Some control centers or IEDs support double channels. The functionality can be
different for each protocol. The links are associations of two channels and they are
used to identify a double channel. Two modes of channels switching are possible:
• AutoSwitch: used with slave protocols. When the active channel stops receiving,
it switches to the other channel, which becomes active
• SwitchByMaster: used with the master protocol, the HU250 controls the channel
switching. A periodic switching between channels can be defined in order to
verify channel state TIME_FORCE_SWITCH
Link copied. Please paste this link to share this article on your social media post.
Hello Milica,
Like always, the devil is in the details so please provide the following a drawing of your communication architecture (from remote SCADA/DMS/ADMS to Easergy T300), including what modems are used (on the IEC 101 and on the IEC 104 links).
Thank you
Link copied. Please paste this link to share this article on your social media post.
@manuellison @JYPOC thank you for your answers.
@JYPOC in attached pictures you can see the project of radio-link. I hope it would be helpful.
Thank you in advance.
Link copied. Please paste this link to share this article on your social media post.
Thank you Milica,
What I was looking for in reality, is the logical communication architecture between the remote SCADA and the T300.
In addition I don't see what is the IEC 101 link here (is it over TCP?).
Regards,
Jean-Yves
Link copied. Please paste this link to share this article on your social media post.
Hi Milica
Would be very useful to know your real application case as requested by Jean-Yves
Is there any legacy habit there?
Generally speaking, it is SCADA/Client responsibility to switch from one channel to another: therefore there is no automatic switching for IEC104/ 101 at T300 level.
The link notion referred by Manuel is applicable to DNP3 protocol
Best Regards
Link copied. Please paste this link to share this article on your social media post.
@JYPOC Yes it is IEC101 over TCP/IP.
@jean-luc_batard Thanks for this the information.
This is old SCADA system at it is still not clear what are the intentions of end customer with IEC101/104. We are still trying to clarify with them what is behind with "transfer link" part. All we know that they want to have two links main and backup: IEC101 serial, and IEC101 over TCP if we understood correctly.
Best regards and thank you very much for help.
Milica Dukic
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.